I want to make a DC meter, which can read DC Voltage and current, with MSP430F427.
Please tell me if it is possible, and if possible please provide details.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to make a DC meter, which can read DC Voltage and current, with MSP430F427.
Please tell me if it is possible, and if possible please provide details.
Thanks in advance.
You may want to look at this post:

It describes a possible input resistor ladder for measuring different voltage levels.
Dennis
Thanks for help Dennis,
My input range is between 0 to 100V and resolution needed is of 10mV.
Previously I have designed volt meter for AC current, but that do not read DC voltage accurately.
So, I need help in reading DC voltage.
Please help.
**Attention** This is a public forum