Hello!
I'm looking for info about DMA. I have MSP432P401 datasheet and also the 432 user guyde.
The datasheet says that there is a 8-channel DMA.
The user guide sems to agree, (fig 9.1). There are 8 channels with 8 possible sources each.
Now when I look at the DMA in the debugger (registers tab), and if I unfold the DMA
label, I can see 32 channels labeled DMA_CHxx_SRCCFG where xx goes from 0 to 31.
Questions:
1. are there 8 or 32 channels? Or is this a bug of the interface?
2. In the debugger, register dab, I can see 32 channekls sources configurations,
Aren't there destination configurations?
3. I don't see any DMA related source code in what I have downloaded. Are there
sanmple programs somewhere? Or someWare?
Thanks,
Pascal