This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Understanding the sample code of Code Composer Studio

I am having trouble understanding the code of Code Composer Studio .


Especially italics part. It would be very helpful if you explain the whole code.

For e,g,


#include "msp.h"
#include "stdint.h"


void error(void);

int main(void)
{
uint32_t currentPowerState;
WDTCTL = WDTPW | WDTHOLD; // Stop WDT


/* NOTE: This example assumes the default power state is AM0_LDO.
* Refer to MSP4322001_pcm_0x code examples for more complete PCM operations
* to exercise various power state transitions between active modes.
*/

/* Step 1: Transition to VCORE Level 1: AM0_LDO --> AM1_LDO */

/* Get current power state, if it's not AM0_LDO, error out */
currentPowerState = PCM->CTL0 & PCM_CTL0_CPM_MASK;
if (currentPowerState != PCM_CTL0_CPM_0)
error();

while ((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_AMR_1;
while ((PCM->CTL1 & PCM_CTL1_PMR_BUSY));
if (PCM->IFG & PCM_IFG_AM_INVALID_TR_IFG)
error(); // Error if transition was not successful
if ((PCM->CTL0 & PCM_CTL0_CPM_MASK) != PCM_CTL0_CPM_1)
error(); // Error if device is not in AM1_LDO mode

/* Step 2: Configure Flash wait-state to 2 for both banks 0 & 1 */
FLCTL->BANK0_RDCTL = FLCTL->BANK0_RDCTL & (~FLCTL_BANK0_RDCTL_WAIT_MASK) | FLCTL_BANK0_RDCTL_WAIT_2;
FLCTL->BANK1_RDCTL = FLCTL->BANK0_RDCTL & (~FLCTL_BANK1_RDCTL_WAIT_MASK) | FLCTL_BANK1_RDCTL_WAIT_2;

/* Step 3: Configure DCO to 48MHz, ensure MCLK uses DCO as source*/
CS->KEY = CS_KEY_VAL ; // Unlock CS module for register access
CS->CTL0 = 0; // Reset tuning parameters
CS->CTL0 = CS_CTL0_DCORSEL_5; // Set DCO to 48MHz
/* Select MCLK = DCO, no divider */
CS->CTL1 = CS->CTL1 & ~(CS_CTL1_SELM_MASK | CS_CTL1_DIVM_MASK) | CS_CTL1_SELM_3;
CS->KEY = 0; // Lock CS module from unintended accesses


/* Step 4: Output MCLK to port pin to demonstrate 48MHz operation */
P4DIR |= BIT3;
P4SEL0 |=BIT3; // Output MCLK
P4SEL1 &= ~(BIT3);

/* Go to sleep */
__sleep();
__no_operation(); // For debugger


}

void error(void)
{
volatile uint32_t i;
P1DIR |= BIT0;
while (1)
{
P1OUT ^= BIT0;
for(i=0;i<20000;i++); // Blink LED forever
}
}

  • Hi Neeraj!

    You forgot to describe what exactly you do not understand / where your problem is located. Please provide some more information!
    For further code postings, please use the Syntaxhighlighter in rich formatting mode which appears on the lower right after clicking on reply.

    Dennis

**Attention** This is a public forum