This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xds200 launchpad mass erase failed

It is really weird.

In a project of mine i'm using the xds200 with the launchpad.

For a very long time it worked, but it seems that since I updated CCS emulators recently (so I moved my xds200 to fw 1.0.0.8), using the debug button can't flash the mcu.

I obtain:

CORTEX_M4_0: GEL Output: Memory Map Initialization Complete
CORTEX_M4_0: GEL Output: Halting Watchdog Timer
CORTEX_M4_0: Flash Programmer: Verbose output enabled
CORTEX_M4_0: Flash Programmer: DLL Version 2.1.1.0
CORTEX_M4_0: Flash Programmer: Hard reset
CORTEX_M4_0: Writing Flash @ Address 0x00000000 of Length 0x00000140
CORTEX_M4_0: Flash Programmer: Uploading RAM loader to device
CORTEX_M4_0: Flash Programmer: Device init finished
CORTEX_M4_0: Flash Programmer: Erasing main memory
CORTEX_M4_0: Flash Programmer: Mass erase failed
CORTEX_M4_0: Flash Programmer: Writing 320 bytes to flash memory 0x00000000
CORTEX_M4_0: Flash Programmer: Write speed 7.4 kB/sec
CORTEX_M4_0: Flash Programmer: Exit flash programming
CORTEX_M4_0: Writing Flash @ Address 0x00001000 of Length 0x00007ff0
CORTEX_M4_0: Flash Programmer: Writing 32752 bytes to flash memory 0x00001000
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Write speed 32.6 kB/sec
CORTEX_M4_0: Flash Programmer: Exit flash programming
CORTEX_M4_0: Writing Flash @ Address 0x00008ff0 of Length 0x00007ff0
CORTEX_M4_0: Flash Programmer: Writing 32752 bytes to flash memory 0x00008ff0
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Write speed 32.8 kB/sec
CORTEX_M4_0: Flash Programmer: Exit flash programming
CORTEX_M4_0: Writing Flash @ Address 0x00010fe0 of Length 0x00004634
CORTEX_M4_0: Flash Programmer: Writing 17972 bytes to flash memory 0x00010fe0
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Verify error. Writing to Flash failed!
CORTEX_M4_0: Flash Programmer: Write speed 32.1 kB/sec
CORTEX_M4_0: Flash Programmer: Exit flash programming
CORTEX_M4_0: Flash Programmer: Hard reset
CORTEX_M4_0: Flash Programmer: Release Watchdog timer

What is strange, is that if I manually connect to the core using the same target configuration, the using the menu Run>Load>Load Program, it works fine:


CORTEX_M4_0: GEL Output: Memory Map Initialization Complete
CORTEX_M4_0: GEL Output: Halting Watchdog Timer
CORTEX_M4_0: Flash Programmer: Erasing main memory
CORTEX_M4_0: Flash Programmer: Writing 320 bytes to flash memory 0x00000000
CORTEX_M4_0: Flash Programmer: Writing 32752 bytes to flash memory 0x00001000
CORTEX_M4_0: Flash Programmer: Writing 32752 bytes to flash memory 0x00008ff0
CORTEX_M4_0: Flash Programmer: Writing 17972 bytes to flash memory 0x00010fe0

It seems to be one project in particular.

That is annoying. Any clue ?

**Attention** This is a public forum