I recently acquired MSP-EXP432p401R launch pad and trying to run some examples. I can successfully connect with CCS6 and debug the OutOfBox_MSP432P401R code. The LED is blinking and changing colors when I press the button, but the GUI is not connecting, even if I close the CCS6.
Also, I tried to run the CC3100BOOST_MQTT-TwitterLED_MSP432P401R example after I connected the CC3100 Booster Pack. The source code builds and loads, but the application hangs on line #140 in device.c. It seems like it's waiting for some bit to change via interrupt and it never happens.
Can anyone help?