I am trying to test a adc12 example code from texas. The code is correct, but when I try to connect a voltage signal at configured adc port the following message appears:
msp430 trouble halting target cpu internal error.
This message appeara when the program is running and i connect the voltage to the pin.
I have revised the erra sheet and schematic to verify that there are not any short.
Can someone help me please? Thanks in advance