Other Parts Discussed in Thread: MSP430FR5969, MSP-EXP430FR5969
I'm in need of an Offscreen image driver for mspware's grlib. It seems like there was support for it at one time, but it has been removed from mspware.
Where are the official repositories of Grlib, and where can I find a supported MSP432 offscreen drive?
There still seem to be some “off screen” remnants in grlib.h
962 extern uint32_t Graphics_getOffscreen1BppImageSize(uint16_t width,
963 uint16_t height);
964 extern uint32_t Graphics_getOffscreen4BppImageSize(uint16_t width,
965 uint16_t height);
966 extern uint32_t Graphics_getOffScreen8BPPSize(uint16_t width, uint16_t height);
and
999 extern void Graphics_initOffscreen1BppImage(Graphics_Display *display,
1000 uint8_t *image, int32_t width, int32_t height);
1001 extern void Graphics_initOffscreen4BppImage(Graphics_Display *display,
1002 uint8_t *image, int32_t width, int32_t height);
1003 extern void Graphics_setOffscreen4BppPalette(Graphics_Display *display,
1004 uint32_t *ppalette, uint32_t offset, uint32_t count);
1005 extern void Graphics_initOffscreen8BppImage(Graphics_Display *display,
1006 uint8_t *image, int32_t width, int32_t height);
1007 extern void Graphics_setOffscreen8BppPalette(Graphics_Display *display,
1008 uint32_t *ppalette, uint32_t offset, uint32_t count);
The getOffscreen ImageSize function are defined in GrLib/grlib/image.c
363:uint32_t Graphics_getOffscreen1BppImageSize(uint16_t width, uint16_t height)
382:uint32_t Graphics_getOffscreen4BppImageSize(uint16_t width, uint16_t height)
401:uint32_t Graphics_getOffScreen8BPPSize(uint16_t width, uint16_t height)
but the initOffscreen Image and setOffscreen Palette functions are defined
in files that are no longer included with the MSPWare Grlib,
but they can be found in the Stellaris and Tiva-c grlib distributions, but those distributions are "older"
in files that are no longer included with the MSPWare Grlib,