This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to convert this code for msp430fr5739

Other Parts Discussed in Thread: MSP430FR5739, L293D, MSP430G2553

#include <msp430fr5739.h>


void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
_delay_cycles(1000000);

// Initialization of the port pins of MSP430G2553 - P1.5 is connected to PIR sensor and the P1.6 and P1.7 are connected to the L293D motor driver
P1DIR |= 0xC1; // Set P1.0 for LED output, P1.6 and P1.7 L293D motor pins to output direction
P1OUT = 0X00;
P2IE |= 0x01; // P2.0 interrupt enabled
P2IES |= 0x01; // P2.0 High/low edge
P2IFG &= ~0x01; // P2.0 IFG cleared

_BIS_SR(LPM4_bits + GIE); // Enter LPM4 w/interrupt
}

// Port 1 interrupt service routine
#pragma <span id="IL_AD7" class="IL_AD">vector</span>=PORT2_VECTOR
__interrupt void Port_2(void)

{
P1OUT ^= 0x01; // P1.0 = toggle

// P1.6 and P1.7 are Enable pins of the L293D (EN1 = 1, EN2 = 0 -- motor rotate in Forward direction)
if(P1OUT & 0x01 == 0x01)
{
P1OUT |= 0x80;
_delay_cycles(1000000);

P1OUT &= ~0xC0; // disable the enable pins to stop the motor
}
// P1.6 and P1.7 are Enable pins of the L293D (EN1 = 0, EN2 = 1 -- motor rotate in Forward direction)
else
{
P1OUT |= 0x40;
_delay_cycles(1000000);

P1OUT &= ~0xC0; // disable the enable pins to stop the motor
}

_delay_cycles(10000);
P2IFG &= ~0x01; // P2.0 IFG cleared
}

**Attention** This is a public forum