Other Parts Discussed in Thread: ENERGIA
Hi,
I am trying to configure the WDT based on the examples provided, wdt_interval_mode, and wdt_service_the_dog
The 432 examples don't change the core frequency, which I guess is 3Mhz.
I readjusted the core frequency to 48Mhz, and to no surprise, the timeout occurs too quickly.
I figured I would just increase the WDT_A_CLOCKITERATIONS_x value by 12, however, on referencing the source code I see that WDT_A_CLOCKITERATIONS_x is a coded value and not a count.
Rather than iteratively try the different and see what happens, does anyone here have a equation for converting code to seconds timeout per core frequency?
These are the choices:
WDT_A_CLOCKITERATIONS_512K -> the wdt example.
WDT_A_CLOCKITERATIONS_8192K
WDT_A_CLOCKITERATIONS_128M
WDT_A_CLOCKITERATIONS_2G