Hello, I'm using a MSP430G2955 in a MSP-TS430DA38 with a 32.768 crystal. I have the program using the using the using the crystal to generate the ACLK and the DCO generating the MCLK and SMCLK at 8Mhz. I am outputting the ACLK on P2.0 and I can see it starts up just fine when I don't have the debugger on. As soon as I try to debug the ACLK slows way down inconsistently (sometimes 1kHz, sometimes 70Hz). I'm using Code Composer Studio 6.1.3.00033 and an old MSP-FET430UIF. I feel like I have the configuration correct because the ACLK starts up reliably if I cycle power but don't run the debugger. Any ideas what this might be?