Other Parts Discussed in Thread: MSP430F1611
Hi,
I'm using a msp430f1611 (w/ Salvo RTOS) and I'm running into some issues with the maximum transfer speed with SPI through UART0. I am using XT2CLK (7.3MHz crystal) for SMCLK and choosing BRCLK to use SMCLK with a divisor of 2. Other relevant SPI registers below:
BCSCTL2 |= SELS; // SMCLK = XTAL2 (7.3728MHz)
ME1 |= USPIE0; //Enable Module
U0CTL |= CHAR + SYNC + MM + SWRST; //SPI, 8-bit data, synchronous mode, master, SWRST
U0TCTL |= CKPH + SSEL1 + SSEL0 + STC; //Use SMCLK for BRCLK, Normal clock phase, 3-pin SPI mode
U0BR0 = 0x02; //Max clock frequency of bus (BRCLK/2)
U0BR1 = 0x00;
U0MCTL = 0x00; //Modulation control not used
U0CTL &= ~SWRST; // Initialize USART state machine
//IE1 = UTXIE0 + URXIE0; //Enable TX and RX interrupts
P3SEL |= BIT1 + BIT2 + BIT3; //this should set up SPI0 to P3_1:3
P3DIR |= BIT0; //Set P3.0 to be GPO to be used for CS in SPI mode
P3OUT |= SPI_CS; //initial state is not selected
I configured all registers to the theoretical maximum SPI clock rate BRCLK/2 (~3.6MHz). Whenever I write to TXBUF0, the data frame shows up twice on the logic analyzer that I am using. I am able to verify that the clock rate is in fact ~3.6MHz. However, when I back the SPI clock rate down to BRCLK/8, the frame only shows up once as it should.
Does anyone have any insight as to what is happening? I am trying to find the max possible spi speed, right now I can only get ~930kHz
Thanks,
Zach