This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432 ADC14 and DMA Usage

Guru 56685 points

With the fast approaching release of MSP432, we have seen an increase in questions/posts about MSP432 on our E2E forums. This has been quite exciting throughout the community and the MSP team to see what great applications the community is already dreaming of with this new device! As result of this enthusiasm, the MSP team has seen increase in requests for software examples for the MSP432. In particular, the usage of ADC14 and the MSP432 DMA, which is a little different from the DMAs of MSP430, has been repeatedly requested in different configurations. This feedback is appreciated and acknowledged with the MSP team working to fulfill some of these and other requests in order to help launch the communities’ development on MSP432. Unfortunately, we cannot fulfill every request, but we do see a need for some additional guidance that is not currently available. The following examples are given to help fill those gaps. These examples may not fill the exact need of your application, but along with the MSP432 TRM and DriverLib API Guide, these examples should help guide you. The MSP team also encourages community members who have similar examples to share here in order to help grow the development power of the community as a whole! Please remember if posting code embedded into a post to use the Rich Text Formatting View link. From here click the </> icon to place code in the code formatter for easier viewing once posted.

This discussion is intended as a resource to supplement the examples for MSP432 that are not available within MSPWare. If you have an issue with using the ADC14 + DMA, beyond requesting for a specific example, please post the issue in a separate thread and not as a reply to this discussion.

Related  ADC14 + DMA E2E Posts:

e2e.ti.com/.../464421

  • The attached example below shows the DMA being used for both ADC (channel 7) and SPI (channel 0).  In both cases the DMA is in 'basic' mode and after each DMA cycle completion the DMA is re-initialized to perform the next transaction.

    /* --COPYRIGHT--,BSD
     * Copyright (c) 2015, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    //****************************************************************************
    //
    // MSP432_DMA_ADC_SPI.c - MSP-EXP432P401R
    //
    //  Port interrupt on P1.1
    //
    //  On port interrupt Send burst via SPI and measure via ADC
    //  Use DMA to load SPI (basic mode Channel 0) and read from ADC (basic mode
    //  channel 7).
    //
    //  UP_SAMPLING        the number of burst/measurements with each button
    //                     press P1.1
    //  TOF_DELAY          delay between SPI burst and ADC measurement
    //  UP_SAMPLING_DELAY  additional delay for each successive burst/measurement
    //                     ie. if UP_SAMPLING is 4 the delays of each measurement
    //                     relative to the spi burst are as follows
    //                     (1) TOF_DELAY+0
    //                     (2) TOF_DELAY+UP_SAMPLING_DELAY
    //                     (3) TOF_DELAY+2*UP_SAMPLING_DLEAY
    //                     (4) TOF_DELAY+3*UP_SAMPLING_DELAY
    //*****************************************************************************
    
    #include "msp.h"
    #include <driverlib.h>
    #include <stdio.h>
    #include <arm_math.h>
    #include "arm_const_structs.h"
    
    #define TOF_DELAY           48          // Based upon SMCLK clock 48Mhz
    
    /*
     * Timer Delay between group of samples.  This number is added to the
     * delay (TOF_DELAY) of subsequent samples.
     */
    #define UP_SAMPLING_DELAY   24
    /*
     * Defines the number of samples to be taken
     */
    #define UP_SAMPLING         4
    #define SAMPLE_LENGTH       128
    #define SAMPLE_FREQUENCY    800000
    
    #define SMCLK_FREQUENCY     48000000
    #define SPI_CLK_FREQUENCY	4000000
    #define SPI_LENGTH			500
    
    /*
     * SPI Configuration Parameter
     * 4Mhz SPI based off of 48MHz SMCLK
     */
    const eUSCI_SPI_MasterConfig spiMasterConfig =
    {
    		EUSCI_B_SPI_CLOCKSOURCE_SMCLK,
    		SMCLK_FREQUENCY,
    		SPI_CLK_FREQUENCY,
            EUSCI_B_SPI_MSB_FIRST,
            EUSCI_B_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT,
            EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, EUSCI_B_SPI_3PIN
    };
    /*
     * TA0 PWM Configuration
     * Timer used to Trigger ADC
     * SMCLK -> SMCLK_FREQUENCY
     * Sample Frequency -> SAMPLE_FREQUENCY
     */
    const Timer_A_PWMConfig pwmConfig =
    {
            TIMER_A_CLOCKSOURCE_SMCLK,              // 48Mhz
            TIMER_A_CLOCKSOURCE_DIVIDER_1,          // 48Mhz
            (SMCLK_FREQUENCY/SAMPLE_FREQUENCY),     // 60
            TIMER_A_CAPTURECOMPARE_REGISTER_1,      // CCR1
            TIMER_A_OUTPUTMODE_SET_RESET,
            (SMCLK_FREQUENCY/SAMPLE_FREQUENCY)/2    // 30
    };
    
    /*
     * TA0 Upmode Configuration
     * Timer used to delay ADC sample relative to SPI burst
     * ACLK -> REFO
     * timerPeriod -> TOF
     */
    Timer_A_UpModeConfig upConfig =
    {
    		.clockSource = TIMER_A_CLOCKSOURCE_SMCLK,
    	    .clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1,
    	    .timerPeriod = TOF_DELAY,
    	    .timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_DISABLE,
    	    .captureCompareInterruptEnable_CCR0_CCIE = TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE,
    	    .timerClear = TIMER_A_SKIP_CLEAR
    };
    
    //40KHZ pulse train
    uint8_t mstxData[SPI_LENGTH] =
    {
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		31,255,255,255,255,255,252,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,0,
    		255,255,255,255,255,255,128,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,128,0,0,0,0,0,
    		31,255,255,255,255,255,252,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		31,255,255,255,255,255,248,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		31,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,128,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,0,
    		255,255,255,255,255,255,192,0,0,0,0,0,
    		31,255,255,255,255,255,252,0,0,0,0,0,0,
    		255,255,255,255,255,255,128,0,0,0,0,0,
    		15,255,255,255,255,255,252,0,0,0,0,0,
    		1,255,255,255,255,255,255,192,0,0,0,0,0,
    		15,255,255,255,255,255,248,0,0,0,0,0,0,0
    };
    
    volatile arm_status status;
    
    /* DMA Control Table */
    #if defined(__TI_COMPILER_VERSION__)
    #pragma DATA_ALIGN(MSP_EXP432P401RLP_DMAControlTable, 1024)
    #elif defined(__IAR_SYSTEMS_ICC__)
    #pragma data_alignment=1024
    #elif defined(__GNUC__)
    __attribute__ ((aligned (1024)))
    #elif defined(__CC_ARM)
    __align(1024)
    #endif
    static DMA_ControlTable MSP_EXP432P401RLP_DMAControlTable[32];
    
    int16_t data_array[UP_SAMPLING][SAMPLE_LENGTH];
    int16_t dataUpSample[UP_SAMPLING*SAMPLE_LENGTH];
    int16_t data_input[SAMPLE_LENGTH];
    
    uint8_t activeCount;
    
    void main(void)
    {
        /* Halting WDT and disabling master interrupts */
        MAP_WDT_A_holdTimer();
        MAP_Interrupt_disableMaster();
    
    /*
     * Debug
     */
    //    memset(data_array,0x0000,SAMPLE_LENGTH);
    //    memset(mstxData,0xFE,500);
    
        /* Set the core voltage level to VCORE1 */
        MAP_PCM_setCoreVoltageLevel(PCM_VCORE1);
    
        /* Set 2 flash wait states for Flash bank 0 and 1*/
        MAP_FlashCtl_setWaitState(FLASH_BANK0, 2);
        MAP_FlashCtl_setWaitState(FLASH_BANK1, 2);
    
        /* Initializes Clock System */
        MAP_CS_setDCOCenteredFrequency(CS_DCO_FREQUENCY_48);
        MAP_CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
        MAP_CS_initClockSignal(CS_HSMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
        MAP_CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1 );
        MAP_CS_initClockSignal(CS_ACLK, CS_REFOCLK_SELECT, CS_CLOCK_DIVIDER_1);
    
        /*
         * Debug, output TA0.1
         */
        P2->DIR |= BIT4;
        P2->SEL0 |= BIT4;
        P2->SEL1 &= ~BIT4;
    
        /*
         * Initializing ADC (MCLK/1/1)
         *
         * 4+16 Clock cycles/conversion -> 417ns
         */
        ADC14_enableModule();
        ADC14_initModule(ADC_CLOCKSOURCE_MCLK, ADC_PREDIVIDER_1, ADC_DIVIDER_1, 0);
    
        ADC14_setSampleHoldTrigger(ADC_TRIGGER_SOURCE1, false);
        /*
         * Setup Sample Pulse mode on ADC14, 4xMCLK sample time, 16xMCLK conversion.
         * When not in use the default is the TA0.1 signal and the sample time is
         * dictated by the high duty cycle.
         */
    //    ADC14->CTL0 |= ADC14_CTL0_SHP;
    //    ADC14->CTL0 &= ~(ADC14_CTL0_SHT1_MASK+ADC14_CTL0_SHT0_MASK);
    
        /* Configuring GPIOs (4.3 A10) */
        MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P4, GPIO_PIN3,
        GPIO_TERTIARY_MODULE_FUNCTION);
        __no_operation();
    
        /* Configuring ADC Memory */
        MAP_ADC14_configureSingleSampleMode(ADC_MEM0, true);
        MAP_ADC14_configureConversionMemory(ADC_MEM0, ADC_VREFPOS_AVCC_VREFNEG_VSS,
        ADC_INPUT_A10, false);
    
        /* Set ADC result format to signed binary */
        //ADC14_setResultFormat(ADC_SIGNED_BINARY);
    
        /*
         * Setup SPI
         */
    
        MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P1,
                GPIO_PIN6, GPIO_PRIMARY_MODULE_FUNCTION);
    
        MAP_SPI_initMaster(EUSCI_B0_BASE, (eUSCI_SPI_MasterConfig*)&spiMasterConfig);
    
        /* Configuring DMA module */
        DMA_enableModule();
        DMA_setControlBase(MSP_EXP432P401RLP_DMAControlTable);
    
        /*
         * Setup the DMA + USCI:SPI interface
         */
        MAP_DMA_setChannelControl(DMA_CH0_EUSCIB0TX0 | UDMA_PRI_SELECT,
        UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_NONE | UDMA_ARB_1);
        MAP_DMA_setChannelTransfer(DMA_CH0_EUSCIB0TX0 | UDMA_PRI_SELECT,
        UDMA_MODE_BASIC, mstxData,
                (void *) MAP_SPI_getTransmitBufferAddressForDMA(EUSCI_B0_BASE),
        		SPI_LENGTH);
    
        DMA_disableChannelAttribute(0,UDMA_ATTR_HIGH_PRIORITY);
        MAP_DMA_assignChannel(DMA_CH0_EUSCIB0TX0);
    
        /*
         * Setup the DMA + ADC14 interface
         */
        DMA_disableChannelAttribute(DMA_CH7_ADC14,
                                     UDMA_ATTR_ALTSELECT | UDMA_ATTR_USEBURST |
                                     UDMA_ATTR_HIGH_PRIORITY |
                                     UDMA_ATTR_REQMASK);
    
        /* Setting Control Indexes. In this case we will set the source of the
         * DMA transfer to ADC14 Memory 0
         *  and the destination to the
         * destination data array. */
        MAP_DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH7_ADC14,
            UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
        MAP_DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH7_ADC14,
        	UDMA_MODE_BASIC, (void*) &ADC14->MEM[0],
            &data_array[0][0], SAMPLE_LENGTH);
    
        DMA_enableChannelAttribute(7,UDMA_ATTR_HIGH_PRIORITY);
    
    
        /* Assigning/Enabling Interrupts */
        MAP_DMA_assignInterrupt(DMA_INT1, 7);
        MAP_Interrupt_enableInterrupt(INT_DMA_INT1);
        MAP_DMA_assignChannel(DMA_CH7_ADC14);
        MAP_DMA_clearInterruptFlag(7);
    
        /* Configuring P1.1 as an input and enabling interrupts */
        MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, GPIO_PIN1);
        MAP_GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1);
        MAP_Interrupt_enableInterrupt(INT_PORT1);
    
        MAP_GPIO_setOutputHighOnPin(GPIO_PORT_P5, GPIO_PIN5);
        MAP_GPIO_setAsOutputPin(GPIO_PORT_P5, GPIO_PIN5);
    
        MAP_Interrupt_enableMaster();
        activeCount = 0;
    
        while(1)
        {
            SCB->SCR |= SCB_SCR_SLEEPDEEP_Pos;
            MAP_Interrupt_enableSleepOnIsrExit();
            MAP_PCM_gotoLPM0();
    
            volatile int i,j;
    
            P5->OUT ^= BIT5;
    		for(i=0; i<SAMPLE_LENGTH; i++)
    		{
    			for(j=0; j<UP_SAMPLING; j++)
    			{
    				dataUpSample[i*UP_SAMPLING+j] = data_array[j][i];
    			}
    		}
            P5->OUT ^= BIT5;
        }
    }
    
    /* Completion interrupt for ADC14 MEM0 */
    #if     __TI_COMPILER_VERSION__ >= 15009000
    __attribute__((ramfunc))
    #endif
    void DMA_INT1_IRQHandler(void)
    {
        /*
         * Stop ADC, SPI, DMA
         */
    
    //    MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P5, GPIO_PIN5);
    	P5->OUT ^= BIT5;
    
        MAP_DMA_disableChannel(0);
        MAP_DMA_disableChannel(7);
    
        MAP_SPI_disableModule(EUSCI_B0_BASE);
        MAP_ADC14_disableConversion();
    
        MAP_ADC14_clearInterruptFlag(ADC14_IFGR0_IFG0);
        MAP_SPI_clearInterruptFlag(EUSCI_B0_BASE,EUSCI_B_IFG_TXIFG0);
        MAP_DMA_clearInterruptFlag(7);
    
        MAP_Timer_A_stopTimer(TIMER_A0_BASE);
    	activeCount++;
        if(activeCount < UP_SAMPLING)
        {
        	//pwmConfig.dutyCycle += UP_SAMPLING_DELAY;
            upConfig.timerPeriod+= UP_SAMPLING_DELAY;
        	/*********************************************************************/
    		/*
    		 * Start Timer to kickoff ADC measurements
    		 */
        	/*********************************************************************/
    		TIMER_A1->CTL &= ~(TIMER_A_CTL_IFG);
    		TIMER_A1->CCTL[0] &= ~(TIMER_A_CCTLN_CCIFG);
    		MAP_Timer_A_configureUpMode(TIMER_A1_BASE,(Timer_A_UpModeConfig*)&upConfig);
    		MAP_Interrupt_enableInterrupt(INT_TA1_0);
    		/*
    		 * Channel 0 Primary
    		 */
    		MSP_EXP432P401RLP_DMAControlTable[0].srcEndAddr = &mstxData[SPI_LENGTH];
    		MSP_EXP432P401RLP_DMAControlTable[0].control =
    				(MSP_EXP432P401RLP_DMAControlTable[0].control & 0xff000000 ) |
    				(((SPI_LENGTH)-1)<<4) | 0x01;
    		MAP_DMA_enableChannel(0);
    		/*
    		 * Channel7 Primary
    		 */
    		MSP_EXP432P401RLP_DMAControlTable[7].dstEndAddr = &data_array[activeCount][SAMPLE_LENGTH];
    		MSP_EXP432P401RLP_DMAControlTable[7].control =
    				(MSP_EXP432P401RLP_DMAControlTable[7].control & 0xff000000 ) |
    				(((SAMPLE_LENGTH)-1)<<4) | 0x01;
    		MAP_DMA_enableChannel(7);
            //MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P5, GPIO_PIN5);
    		MAP_SPI_enableModule(EUSCI_B0_BASE);
    		//MAP_Timer_A_startCounter(TIMER_A0_BASE,TIMER_A_UP_MODE);
    		TIMER_A1->CTL |= TIMER_A_CTL_MC__UP;
        	/*********************************************************************/
        }
        else
        {
            MAP_Interrupt_disableSleepOnIsrExit();
            activeCount = 0;
            upConfig.timerPeriod = TOF_DELAY;
        }
    	P5->OUT ^= BIT5;
    }
    
    /* GPIO ISR */
    #if     __TI_COMPILER_VERSION__ >= 15009000
    __attribute__((ramfunc))
    #endif
    void PORT1_IRQHandler(void)
    {
        uint32_t status;
    
        status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P1);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, status);
    
        /* Toggling the output on the LED */
        if(status & GPIO_PIN1)
        {
            /*
             * Start ADC, SPI, DMA
             */
            //MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P5, GPIO_PIN5);
        	P5->OUT ^= BIT5;
        	while(status & GPIO_PIN1)
        	{
        	    status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P1);
        	    MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, status);
        	}
    
            /*
             * Start Timer to kickoff ADC measurements
             */
        	/*********************************************************************/
            TIMER_A1->CTL &= ~(TIMER_A_CTL_IFG);
            TIMER_A1->CCTL[0] &= ~(TIMER_A_CCTLN_CCIFG);
            MAP_Timer_A_configureUpMode(TIMER_A1_BASE,(Timer_A_UpModeConfig*)&upConfig);
            MAP_Interrupt_enableInterrupt(INT_TA1_0);
            /*
             * Channel 0 Primary
             */
    		MSP_EXP432P401RLP_DMAControlTable[0].srcEndAddr = &mstxData[SPI_LENGTH];
        	MSP_EXP432P401RLP_DMAControlTable[0].control =
        			(MSP_EXP432P401RLP_DMAControlTable[0].control & 0xff000000 ) |
    				(((SPI_LENGTH)-1)<<4) | 0x01;
            MAP_DMA_enableChannel(0);
        	/*
        	 * Channel7 Primary
        	 */
        	MSP_EXP432P401RLP_DMAControlTable[7].control =
        			(MSP_EXP432P401RLP_DMAControlTable[7].control & 0xff000000 ) |
        			(((SAMPLE_LENGTH)-1)<<4) | 0x01;
            MAP_DMA_enableChannel(7);
            //MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P5, GPIO_PIN5);
        	P5->OUT ^= BIT5;
            MAP_SPI_enableModule(EUSCI_B0_BASE);
            //MAP_Timer_A_startCounter(TIMER_A0_BASE,TIMER_A_UP_MODE);
            TIMER_A1->CTL |= TIMER_A_CTL_MC__UP;
        	/*********************************************************************/
        }
    }
    
    /* TA1_0 ISR */
    #if     __TI_COMPILER_VERSION__ >= 15009000
    __attribute__((ramfunc))
    #endif
    void TA1CCR0_IRQHandler(void)
    {
        //MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P5, GPIO_PIN5);
    	P5->OUT ^= BIT5;
        //MAP_Timer_A_stopTimer(TIMER_A0_BASE);
    	TIMER_A1->CTL &= ~TIMER_A_CTL_MC_3;
        MAP_ADC14_enableConversion();
    	MAP_Timer_A_generatePWM(TIMER_A0_BASE, &pwmConfig);
        //MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P5, GPIO_PIN5);
    	P5->OUT ^= BIT5;
    	TIMER_A1->CCTL[0] &= ~(TIMER_A_CCTLN_CCIFG+TIMER_A_CCTLN_CCIE);
    	MAP_Interrupt_disableInterrupt(INT_TA1_0);
    }
    

  • The ADC and DMA can be implemented in a number of ways in the following example. In the ADC ISR, three DMA transfers are started to capture the data from three ADC channels. The ping-pong method is used and after 'n' samples of each channel have been collected the DMAs need to be serviced. The ADC is timer triggered and in autoscan mode (not shown).

    /*
    * This interrupt is fired whenever the sequence is completed
    *
    */
    __attribute__((ramfunc))
    void ADC14_IRQHandler(void)
    {
    uint64_t status;
    // Turn on LED
    
    // Toggle at 12Khz frequency, look like 6khz clock
    //MAP_GPIO_setOutputHighOnPin(GPIO_PORT_P1, GPIO_PIN0);
    P1OUT |= BIT0;
    
    status = ADC14_getEnabledInterruptStatus();
    MAP_ADC14_clearInterruptFlag(status);
    if(status & ADC_INT8)
    {
    MAP_ADC14_disableConversion();
    /* Forcing a software transfer on DMA Channel 0 */
    MAP_DMA_requestSoftwareTransfer(0);
    /* Forcing a software transfer on DMA Channel 1 */
    MAP_DMA_requestSoftwareTransfer(1);
    /* Forcing a software transfer on DMA Channel 2 */
    MAP_DMA_requestSoftwareTransfer(2);
    
    MAP_ADC14_enableConversion();
    }
    //MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    P1OUT &= ~BIT0;
    }
    
    /* Completion interrupt for ADC14 MEM6 */
    __attribute__((ramfunc))
    void DMA_INT1_IRQHandler(void)
    {
    /* Switch between primary and alternate bufferes with DMA's PingPong mode */
    if (DMA_getChannelAttribute(0) & UDMA_ATTR_ALTSELECT)
    {
    DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH0_RESERVED0,
    UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH0_RESERVED0,
    UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[6],
    prim_buffer0, NUMBER_OF_SAMPLES);
    }
    else
    {
    DMA_setChannelControl(UDMA_ALT_SELECT | DMA_CH0_RESERVED0,
    UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    DMA_setChannelTransfer(UDMA_ALT_SELECT | DMA_CH0_RESERVED0,
    UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[6],
    alt_buffer0, NUMBER_OF_SAMPLES);
    }
    // Toggle at 512 measures of adc6
    MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P2, GPIO_PIN0);
    }
    
    /* Completion interrupt for ADC14 MEM7 */
    __attribute__((ramfunc))
    void DMA_INT2_IRQHandler(void)
    {
    /* Switch between primary and alternate bufferes with DMA's PingPong mode */
    if (DMA_getChannelAttribute(1) & UDMA_ATTR_ALTSELECT)
    {
    DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH1_RESERVED0,
    UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH1_RESERVED0,
    UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[7],
    prim_buffer1, NUMBER_OF_SAMPLES);
    }
    else
    {
    DMA_setChannelControl(UDMA_ALT_SELECT | DMA_CH1_RESERVED0,
    UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    DMA_setChannelTransfer(UDMA_ALT_SELECT | DMA_CH1_RESERVED0,
    UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[7],
    alt_buffer1, NUMBER_OF_SAMPLES);
    }
    // Toggle at 512 measures of adc7
    MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P2, GPIO_PIN0);
    }
    
    /* Completion interrupt for ADC14 MEM8 */
    __attribute__((ramfunc))
    void DMA_INT3_IRQHandler(void)
    {
    /* Switch between primary and alternate bufferes with DMA's PingPong mode */
    if (DMA_getChannelAttribute(2) & UDMA_ATTR_ALTSELECT)
    {
    DMA_setChannelControl(UDMA_PRI_SELECT | DMA_CH2_RESERVED0,
    UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    DMA_setChannelTransfer(UDMA_PRI_SELECT | DMA_CH2_RESERVED0,
    UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[8],
    prim_buffer2, NUMBER_OF_SAMPLES);
    switch_data = 1;
    }
    else
    {
    DMA_setChannelControl(UDMA_ALT_SELECT | DMA_CH2_RESERVED0,
    UDMA_SIZE_16 | UDMA_SRC_INC_NONE | UDMA_DST_INC_16 | UDMA_ARB_1);
    DMA_setChannelTransfer(UDMA_ALT_SELECT | DMA_CH2_RESERVED0,
    UDMA_MODE_PINGPONG, (void*) &ADC14->MEM[8],
    alt_buffer2, NUMBER_OF_SAMPLES);
    switch_data = 0;
    }
    // Toggle at 512 measures of adc8
    MAP_GPIO_toggleOutputOnPin(GPIO_PORT_P2, GPIO_PIN0);
    //MAP_Interrupt_disableSleepOnIsrExit();
    SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Pos;
    }
    
    ---------------------------------------------------------------------------------------------------------

  • Another example of DMA+ADC on MSP432 can be seen within the Educational Boosterpack MicrophoneFFT example shown here:

    http://dev.ti.com/tirex/#/?link=MSPWare%2FDevelopment%20Tools%2FMSP-EXP432P401R%2FDemos%2FBoosterPack%20Demos

  • Additional information pertaining to ADC14 + DMA and errata, see the following post:

    e2e.ti.com/.../1920081
  • This example is almost exactly what I would like to do! 

    Unfortunately, I can't get it to build properly; I just started dabbling with the MSP432 a day or two ago, so am not up to speed yet, but it feels like I'm missing something super obvious. I have done the following:

    • I imported the driverlib_empty_project from the Resource Explorer
    • It couldn't find msp.h, but i was able to include it from ti/ccsv7/ccs_base/arm/include
    • It couldn't find driverlib.h, but i was able to include it from ti\simplelink_msp432_sdk_1_40_00_28\source\ti\devices\msp432p4xx\driverlib
    • It cannot find arm_math.h and apparently that file is not included in the simplelink source or ccs anywhere

    Am I missing some toolkit? I've read that it's best to start from a working example project rather than trying to start your own, so I assume there's a few key items that need to be included from somewhere, somehow.

    Additionally, I was unable to find any of the DMA examples that seem to be vaguely referenced on this forum in the Resource Explorer, including, for example, the microphone booster pack one.

    Hopefully somebody can enlighten me? 

    Julian

  • I have managed to get the previous single channel file running; I'm still a little unclear as to how to set up the interrupts, triggering and autoscan stuff for multichannel DMA; could you show how you set up these for the above?

  • Thanks, Could you also mention any good reference material for knowing more about MSP432 controllers.
  • To those following this thread:

    This thread is supposed to be an information dump for MSP432 DMA + ADC information. If you have additional questions, please start a new E2E thread.

**Attention** This is a public forum