Hi all,
I am using MSP-TS430REU128 USB board with MSP430F6779A controller. I am getting the following error on CCS Version: 6.1.3.00033 , "error initializing emulator: Your connected hardware might drain too much power from the debugger. This results in an overcurrent." Tried to update the firmware(as suggested) but it would not even do that.
I just have a crystal connected to controller, there is nothing else connected to it. I faced this problem earlier and had to restart my system and it worked. Now even after restarting the system several times it does not work. I am working on Windows 10.
Any help would be appreciated, thank you.