I'm designing my own boosterpack board for MSP432 LaunchPad now.
I noticed that I need special connector to connect it with MSP432 LaunchPad.
What I need is
CONN HEADER 20POS .100" DUAL, FEMALE with long male leads CNT-F254-2*10-GS-850-9
I find the link to the store all right.
http://www.retrodesignlab.com/LaunchPad/store/#!/CRD-081413-A-F/p/29462048/category=6922288
CRD-081413-A-F
2x10 female socket
2.54mm pitch
Through hole straight type
Gold Flash Plated
$0.56
It's cheap! I need two CRD-081413-A-F = $1.12 all right.
But I must pay $86.74 for shipping them to Japan!
Are there any compatible connector, which I can purchase at RS-Components or Digi-key?
I don't want to spent so much money as shipping cost!