This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C PROBLEM IN MSP430G25553

Other Parts Discussed in Thread: MSP430G2553, TMP102, BQ76940

HI, I`m in a fight with i2c of MSP430G2553, and i saw a lot of answers but big part without a good explanation of problem.  To try solve it and help other users of MSP430G2553 I WILL POST MY QUESTION AND WISH SOMEONE CAN HELP US. 

INFORMATIONS: 

COMPILER CCS 

I`M USING THE MSP430G2553 TO READ THE SENSOR TMP102 AND M24LR, I STARTED USING MSPWARE EXAMPLE IN THIS EXAMPLE msp430g2xx3_usci_i2c_master_tx in  example the IC2 COMMUNICATION USES interrupt mode to works and show the communication between two MSP devices. 

in my project i want to use I2C in polling mode. and generate functions like :

int I2CSendByte(unsigned char I2CSlaveAddress, unsigned char data)

int I2CWriteRegisterByte(unsigned char I2CSlaveAddress, unsigned char Register, unsigned char Data)

I found a document of TI with i2c communication with bq76940 (http://www.ti.com/lit/an/slva626b/slva626b.pdf ) and 

) and in all codes tested  i found the same problem, the flag IFG didnt change the state: Below my code: 

void I2C_Init(void)
{

P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0, P1.6 for SCL and P1.7 for SDA
P1SEL2|= BIT6 + BIT7; // Assign I2C pins to USCI_B0, P1.6 for SCL and P1.7 for SDA

UCB0CTL1 |= UCSWRST; // PUT I2C control in logic reset (register = 0x01)
UCB0CTL0 = UCMODE_3 + UCSYNC; //USMODE_3 = 0x06 = I2C MODE UCSYNC = 0x01 ( I2C + SYNC MODE)
UCB0BR0 = 20;
UCB0BR1 = 0;

UCB0I2CIE = 0;
IE2 &= ~(UCB0TXIE + UCB0RXIE); //disable interrupts
UCB0I2CIE |= UCNACKIE; // Interrupt on slave Nack
UCB0CTL1 |= UCSSEL_2;
UCB0CTL1 &= ~UCSWRST;

}

int I2CSendByte(unsigned char I2CSlaveAddress, unsigned char data)
{
unsigned long int DelayCounter = 0;

UCB0CTL0 |= UCMST;
UCB0I2CSA = I2CSlaveAddress;

UCB0CTL1 |= UCTR; //data in transmit direction
UCB0CTL1 |= UCTXSTT; //Generate Start Condition
//Send Start Byte

while(!(IFG2 & UCB0TXIFG)) //if UCB0TXIFG != 0, wait here
{
DelayCounter ++;
if (UCNACKIE ==1)
{
DelayCounter = 55;
return -2;
}
if (DelayCounter >= DELAY_LIMIT)
break;
}

if (DelayCounter >= DELAY_LIMIT)
return -1;

UCB0TXBUF = data; // send the data

DelayCounter = 0;

while(DelayCounter < DELAY_LIMIT && !(IFG2 & UCB0TXIFG))
{
DelayCounter++;
}

if (DelayCounter >= DELAY_LIMIT)
return -1;

UCB0CTL1 |= UCTXSTP; //send stop bit

DelayCounter = 0;

while(DelayCounter < DELAY_LIMIT && (UCB0CTL1 & UCTXSTP))
{
DelayCounter++;
}

if (DelayCounter >= DELAY_LIMIT) //check if NACK condition occurred
return -1;
else
return 0;
}

the problem is in line while(!(IFG2 & UCB0TXIFG)) //if UCB0TXIFG != 0, wait here inside of fuction I2CSendbytes. 

Somebody can help solve this problem, and explain me why it happen. 

Thanks for your attention and with this code working I will share same in group to avoid this question again 

  • If no software works, it's probably a hardware problem. Show your circuit.
  • attached the wave form of I2C signal and the point where the firmware  freeze. 

    Attached the last code in test, same problem 

    
    
    /********************************************************************************************/
    /*    Include                                                                               */
    /********************************************************************************************/
    #include	"msp430g2553.h"
    
    /********************************************************************************************/
    /*    I2C Definitions                                                               	    */
    /********************************************************************************************/
    //I2C Port Definitions
    #define   i2cAddress     0x48    //Address GPIO Address
    #define   I2C_ADDR_TMP   0x48	// address temperature sensor m24LR64
    #define   I2C_ADDR_M24   0x50	// address RFID tag sensor
    
    //USCI I2C PIN Definition
    #define   SDA_PIN     BIT7		//Bit 7 USCI Port 1(SDA)
    #define   SCL_PIN     BIT6		//Bit 6 USCI Port 1(SCL)
    
    
    /********************************************************************************************/
    /*    UART Function Definitions                                                                  */
    /********************************************************************************************/
    
    void UART_puts(char * s);
    void UART_outdec(long data, unsigned char ndigits);
    
    /********************************************************************************************/
    /*    I2C Function Definitions  												                */
    /********************************************************************************************/
    void I2C_Write_M24LR_TMP(unsigned char slave_address, unsigned int register_address, char * data, unsigned char DataLength );
    void I2C_Read_M24LR_TMP(unsigned char slave_address, unsigned int memory_address, char * data, unsigned char DataLength );
    
    
    /********************************************************************************************/
    /*    Misc Function Definitions                                                                  */
    /********************************************************************************************/
    void delay_ms(unsigned int delay);			//Delay
    
    
    /********************************************************************************************/
    /*   Main                                                                  */
    /********************************************************************************************/
    void main(void) {
    
    	WDTCTL = WDTPW + WDTHOLD;		  	// Stop WDT
    
    	BCSCTL1 = CALBC1_16MHZ;				//set DCO to 16Mhz
    	DCOCTL = CALDCO_16MHZ;				// make sure to update the Delay_ms function if the DCO is changed
    
    
    	//UART Initial
    	P1SEL = BIT1 + BIT2;                     // P1.1 = RX pin, P1.2=TX pin
    	P1SEL2 = BIT1 + BIT2 ;                    // P1SEL and P1SEL2 = 11--- Secondary peripheral module function is selected.
    	UCA0CTL1 |= UCSSEL_2;                     // SMCLK
    	UCA0BR0 = 69;                             // 16MHz 230400
    	UCA0BR1 = 0;                              // 16MHz 230400
    	UCA0MCTL = UCBRS0;                        // Modulation UCBRSx = 1
    	UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
    	IE2 |= UCA0RXIE;                          // Enable USCI_A0 RX interrupt
    
    	//USCI_I2C_Init
    	P1SEL |= SDA_PIN + SCL_PIN;						// Assign I2C pins to USCI_B0
    	P1SEL2|= SDA_PIN + SCL_PIN;
    	UCB0CTL1 = UCSWRST;								// Enable SW reset, HOLD USCB in a reset state
    	UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;			// I2C Master, MODE 3 = I2C, synchronous mode
    	UCB0CTL1 = UCSSEL_2 + UCSWRST;					// Use SMCLK, keep SW reset
    	UCB0BR0 = 72;									// Set I2C master speed  72 gives approx 200Khz clock at 16Mhz
    	UCB0BR1 = 0;									// Set I2C master speed
    	UCB0CTL1 &= ~UCSWRST;							// Clear SW reset, resume operation
    
    
    	UART_puts("Starting...\r\n");		//output to UART to indicate the program is running
    
    //	__bis_SR_register(CPUOFF + GIE);        							// LPM0 with interrupts enable
    	    __bis_SR_register(GIE);
    		while (1){
    
    			I2C_Write_M24LR_TMP(I2C_ADDR_TMP,0x00,"ABCDEFGHIJKLMNOP",15);
    
    		}
    
    
    
    
    
    
    
    
    }
    
     void UART_puts(char * s) {
     	while (*s) {
     		while (!(IFG2 & UCA0TXIFG));                // USCI_A0 TX buffer ready?
     		UCA0TXBUF = *s++;
     	}
     }
    
    
     void UART_outdec(long data, unsigned char ndigits){  	//UART_outdec modified/hacked to properly handle negative numbers.
     	unsigned char sign, s[15];			//I copied this from a TI example or the 40oh forum, but I'm not sure of the original author.
     	unsigned int i;
     	sign = 0x00;
    
     	if(data < 0) {
     		sign='-';
     		data = -data;
     	}
     	i = 0;
    
     	do {
     		s[i++] = data % 10 + '0'; //adds the value of data least sig digit to ascii value of '0'
     		if(i == ndigits) {
     			s[i++]='.';
     		}
     	} while( (data /= 10) > 0);
    
     	if (i < ndigits) //fixes loss of leading 0 in fractional portion when number of digits is less than length of data
     	{
     		do {
     			s[i++]='0';
     			} while (ndigits > i) ;
    
     		s[i++]='.';
     	}
    
     	if (sign == '-')  //if value is negative then include the '-' sign
     	{
     		s[i] = sign;
     	} else
     	{			//if value is positive then reduce 'i' counter by 1 to prevent the do loop from trying to output a sign character.
     		i--;
     	}
    
     	do {
     		while (!(IFG2 & UCA0TXIFG));
     		UCA0TXBUF = s[i];
     	} while(i--);
     }
    
    
    
    
     void delay_ms(unsigned int delay)
     {
         while (delay--)
         {
             __delay_cycles(16000);  //1ms = 1000 cycles per 1Mhz clock freq.
         }
     }
    
    
    void I2C_Read_M24LR_TMP(unsigned char slave_address, unsigned int memory_address, char * data, unsigned char DataLength )
    { //Reading from a 24LCxxx series is much easier then writing.  Reading doesn't have to be done in 64 byte pages.
    	/*
    		 * Todo:
    		 * 1. add checks to make sure write does not exceed maximum length of EEprom
    		 * 2. check for valid memory_address
    		 *
    		 */
    
    	int rLoop = 0;	//loop counter
    
    	while (UCB0STAT & UCBBUSY);			//wait for USCI B0 bus to be inactive
    	UCB0I2CSA = slave_address;			//set SLAVE address
    
    	UCB0CTL1 |= UCTR + UCTXSTT;						//set USCI to be I2C TX,  send start condition
    	UCB0TXBUF = (memory_address & 0x7F00) >> 8;		//transfer memory_address MSB
    
    	while (UCB0CTL1 & UCTXSTT);						// waiting for slave address to transfer
    	while ((IFG2 & UCB0TXIFG) != UCB0TXIFG);		//wait for TX IFG to clear
    
    	UCB0TXBUF = (memory_address & 0x00FF);			//transfer memory_address LSB
    	while ((IFG2 & UCB0TXIFG) != UCB0TXIFG);		//wait for TX IFG to clear
    
    	UCB0CTL1 &= ~UCTR;  			//set USCI to be RECEIVER
    	UCB0CTL1 |= UCTXSTT; 			//send restart
    	while (UCB0CTL1 & UCTXSTT);		// wait until I2C STT is sent
    
    	for (rLoop=0; rLoop<DataLength; rLoop++)	//receive loop
    	{
    		 while ((IFG2 & UCB0RXIFG) != UCB0RXIFG); //wait for RX buffer to have data
    		    data[rLoop] = UCB0RXBUF;  //Move rvcd data of or USCI buffer. This also clears the UCB0RXIFG flag
    
    		    if (rLoop == DataLength-2) 	//NACK and STOP must be send before the last byte is read from the buffer.
    		    							//if not the CPU will read an extra byte.
    		    {
    		    	UCB0CTL1 |= UCTXNACK; //generate a NACK
    		    	UCB0CTL1 |= UCTXSTP;  //generate a stop condition
    		    }
    	}
    
    
    }
    
    void I2C_Write_M24LR_TMP(unsigned char slave_address, unsigned int memory_address, char * data, unsigned char DataLength )
    {
    	/*
    	 * Todo:
    	 * 1. add checks to make sure write does not exceed maximum length of EEprom
    	 * 2. check for valid memory_address
    	 *
    	 */
    
    
    	int NumPages = (DataLength)/64 ; //Count of full 64 byte pages, 0 means the data is less than a full 64 byte page
    	int PartialPageBytes = DataLength % 64;  //this is the number of bytes remaining that do not make up a full page
    
    	int address = 0; //EEprom memory starting address, this is different from the I2C slave address
    	int NP =1; //loop counter to iterate though pages of memory
    	int offset = 0;
    	int offsetlimit = 0;
    
    	if (PartialPageBytes > 0)
    	{
    		NumPages++; //if we have left over bytes that do not make up a full page, this will add a page to handle those bytes.
    	}
    
        __disable_interrupt(); //prevent interrupts from messing with the I2C functions
    
    	while (UCB0STAT & UCBBUSY);		//wait for USCI B0 bus to be inactive
    	    	UCB0I2CSA = slave_address;			//set SLAVE address
    
        for (NP=1; NP<=NumPages; NP++)
    	{
    
    		address = ((NP-1) * 64) + memory_address; //this is the full page start address
    
    		UCB0CTL1 |= UCTR + UCTXSTT;			//set USCI to be I2C TX,  send start condition
    		UCB0TXBUF = (address & 0x7F00) >> 8;		//transferring memory_address MSB
    
    		while (UCB0CTL1 & UCTXSTT);					// waiting for slave address was transferred
    		while ((IFG2 & UCB0TXIFG) != UCB0TXIFG);		//wait for TX IFG to clear
    
    	    UCB0TXBUF = (address & 0x00FF);		//transferring memory_address LSB
       	    while ((IFG2 & UCB0TXIFG) != UCB0TXIFG);		//wait for TX IFG to clear
    
       	    offsetlimit = 63; 		//set the offset limit to 63
    
       	    if ((NP == NumPages) && (PartialPageBytes > 0))		//if we are preparing to send the last/partial page
       	    {
       	    	offsetlimit = PartialPageBytes-1;				//set the offset limit to the number of partial page bytes
       	    }
    		for (offset=0; offset <=offsetlimit; offset++)
    		{
    			UCB0TXBUF = data[((NP-1)*64)+offset];					//send data.
    			//UART_outdec(offset,0);
    
    			while ((IFG2 & UCB0TXIFG) != UCB0TXIFG);	//wait for TX IFG to clear
    
    		}
    
    		UCB0CTL1 |= UCTXSTP;                    // set I2C stop condition
    		while ((UCB0STAT & UCSTPIFG) == UCSTPIFG); //wait for Stop condition to be set
    
    						//delay while the EEPROM completed its write cycle.
    						//It would be better to use NACK polling here as described in the datasheet.
    	    delay_ms(6); 	//24LC256 has a max page write time of 5ms, so we will wait 6ms to be sure
    	}
    
    	UART_puts("Done...\r\n");
    	__enable_interrupt();
    
    }
    
    
    // -----------------------------------------------------------------------------
    // Interrupt Handlers
    // -----------------------------------------------------------------------------
    
    
    #pragma vector=USCIAB0RX_VECTOR
    __interrupt void USCI0RX_ISR(void)
    {
    	__bic_SR_register_on_exit(CPUOFF);        // Clear CPUOFF bit from 0(SR)
    
    	char RxChar = 0x00; //char used to receive serial data
    	RxChar = UCA0RXBUF;                    // copy the RX buffer into RxChar
    
    	char buf[4] = {0};  //i2c received data buffer
    
    
    	//void I2C_Write_EEProm(unsigned char slave_address, unsigned int memory_address, char * data, unsigned char DataLength )
    	I2C_Write_M24LR_TMP(i2cAddress,0x00,"ABCDEFGHIJKLMNOP",15);
    
    	//void I2C_Read_EEProm(unsigned char slave_address, unsigned int memory_address, char * data, unsigned char DataLength )
    	I2C_Read_M24LR_TMP(i2cAddress,0x05,buf,5);  //reads three bytes starting at memory location 0x05 and returns the data into 'buf'
    	UART_puts("READING: \r\n");
    	UART_puts(buf);
    	UART_puts("\r\n");
    
    
    
    	__bis_SR_register(CPUOFF + GIE);        							// LPM0 with interrupts enable
    
    } //end UART RCV ISR
    


    /

  • I have nothing to add to my previous post.

**Attention** This is a public forum