Hello everyone,
I am using IAR Embedded Workbench ARM version 7.70.1.11486 for programming MSP432P401R launchpad. I tried to run the sample code of LED blinking provided in slau574c document. But after clicking on "Download & Debug" it gives Fatal error: Failed to Load the CPU Core Driver Session aborted. The program had compiled successfully.
The message is as follows:
IAR Embedded Workbench 7.70.1 (armproc.dll)
Loaded macro file: D:\arm\config\debugger\TexasInstruments\MSP432P401R.dmac
Loaded macro file: D:\arm\config\flashloader\TexasInstruments\FlashMSP432P4.mac
Connecting to TI XDS110 ( Probe no: 00000000 ) COM[18/17]
Fatal error: Failed to load the CPU core driver Session aborted!
Unloaded macro file: D:\arm\config\flashloader\TexasInstruments\FlashMSP432P4.mac
IAR Embedded Workbench 7.70.1 (armproc.dll)
I am using TI-XDS110 onboard debugger and followed the steps which are mentioned in the document.
Use Flash LOader option is selected in Download tab.
Would be great if someone helps me with this, I tried a lot to find out ways of solving it but couldn't do it.
Thanks in advance.