This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What's the internal resistor accuracy for the MSP432



Hi Dung,

What's the internal resistor accuracy for the MSP432? The reason is that If we can't get the 0.1%, 25ppm external DCOR, would it possible we use a 0.5% or 1% DCOR and still better than using the internal resistor.

  • Hi Louis,

    Resistor accuracy will get directly added to the time period accuracy. For ex DCO accuracy is specified assuming Ext R has 0% tolerance, lets say its X%.

    Time period is prop to RC product. Hence Y% tolerance in R will directly come out at DCO and DCO will have X+Y % accuracy.

    In other words, we can say that while this is not specified, R accuracy is additive to overall DCO accuracy.

    Hopefully this helps.

    David
  • Hi David,

    Thanks for the reply. The reason that I ask this is because customer don't have a 0.1% 91K resister. So we would like to know what result we would expect if we use a 0.5%? 0.2% resistor, is it linear compared to 0.1%.

    Thanks.
  • Hi Louis,

    Yes that should be the case. In general, we can say that while this is not specified, R accuracy is additive to overall DCO accuracy. So if external R is 0.1% + X% therefore DCO accuracy is datasheet spec + X%.

    Regards,

    David

**Attention** This is a public forum