Dear all,
I want to design a constant current source of 10 mA which will not vary on load connected.
Is there any IC available for it?
My load will vary from 10 ohm to 5k ohm.
I have tried using discrete components (Howland current source but i unable to achieve 10mA current. Howland source gives me 5.2mA constant current at 12V voltage)
Please suggest me good circuit or IC
I have attached the circuit which i simulated. if I change the value of resistances below 2.3k then current is not getting constant through 5K load