Other Parts Discussed in Thread: MSP430-GCC-OPENSOURCE
Hello!
I'm trying to setup a new CCS project using MSP430 GCC.
1. When I go to app center, the button at the right bottom of GCC says "up to date",
so I guess I don't have to install or update anything.
2. When I try to make a new program:
File->New->CCS project. The setup window opens.
As I use the 5529 launchpad, I type 5529 in the target filter, and there is a single
candidate that I can select.
Then I set a project name and choose a location.
Now trying to choose a compiler, but there is only TIv15.12.1.LTS
Does anybody know how to start a MSPGCC project using CCS?
Thanks,
Pascal