This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
I am using the MSP430F5419 MCU on a design for a supervisory and communication function. The main system is running on an i.MX6 application processor on a single-board computer using Linux.
If talking with the MSP430 running our custom application code, and then we try to run the BSL update program, it would fail. If we reboot the entire system and then enter and communicate with the bootloader before ever talking UART to our application code, then it works fine. We can then run application code and the bootloader file load will be successful.
In an attempt to determine whether or not this was a Linux interface issue, we even integrated the entire bootloader program into our application software on the HMI side, and even then we had the exact same problem.
Can you offer some insight into why this would be and how we can better understand this problem so we can work around it or resolve it?
Any feedback or input is welcomed and appreciated!
Thanks again!
Paul
Hi Paul,
According to Section 6.5 Bootstrap Loader (BSL) in the datasheet, usage of the BSL on this device requires 4 pins (see Table 6-3), and the BSL entry requires a specific entry sequence on the ~RST/NMI/SBWTDIO and TEST/SBWTCK pins. If the interface between the application processor and the MSP430 only includes two UART RX/TX pins (and not the additional ~RST/TEST pins), there's no way for the BSL entry sequence to start properly without powering cycling the entire system.
Take a look at Section 1.3 Standard RESET and BSL Entry Sequence in the MSP430 Programming With the Bootloader (BSL) app note for the appropriate entry sequence for this device.
Let me know if this doesn't make sense.
Regards,
James
MSP Customer Applications
Thanks James!
We are very familiar with that application note as we reviewed it in great detail. We also believe that we have followed the BSL entry procedure. We have control over the RST and TST pins. We don't believe that is our issue. Our issue is that, for whatever reason, we seem to be unable to communicate with the BSL over UART if we have previously been talking over the UART to application code running on the MSP430. If we handle the BSL first, then later talk to the application, things are fine. We only brought it up because we were previously having no issue talking to the BSL at any point. We did change the board that talks to the MSP430, but the circuitry is equivalent/identical. I could provide schematics if you would like.
Paul
Hi Paul,
This is strange, especially since the circuitry hasn't changed. Perhaps, this is a timing issue on the entry sequence or a parity issue? Since this is a different board, it could be running faster than the previous board. Make sure the baud rate is at 9600 (or very close to this), as discussed in the NOTE on page 6 here. Also, keep in mind that the minimum time delay before sending new characters after characters have been received from the MSP430 BSL is 1.2 ms.
Regarding the parity bit, it doesn't look like the BSL on the MSP430F5419 expects a parity bit (discussed on page 42 here), so if you're using even parity for your general UART communication, this could be a problem.
Regards,
James
MSP Customer Applications
**Attention** This is a public forum