This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As per the datasheet, it looks like there is no buffer provision when Vcc is selected as Vr+ i.e. SREFx=0 in ADC10CTL0 register. Hence, the sampling time would be only dependent on the following formula: tsample > (RS + RI) × ln(2^11) × CI and not the tREFBURST, is this understanding correct? Thank you.
**Attention** This is a public forum