Other Parts Discussed in Thread: MSP430G2553, ENERGIA, MSPDS
Hello I recently purchased a MSP-EXP430G2 Launchpad. I have been using CCS V6.1.1 with the F28M36. I need a simpler chip for my current projects and the MSP430 seems to meet my needs and allows me to continue using CCS with TFS.
I am having issues getting the basic blink led to run. I keep getting a "Error initializing emulator: No USB FET was found" Solved wrong driver it needs "MSP Debug Interface"
I have searched the forum and watched some videos on line and have yet to find an answer some posts are quite old....
I did not originally have the MSP430 device installed with CCS, I have run installation again and added those tools.
I even tried the Cloud version with no success.
Questions:
When I look at Device Manager I see MSP-430F5438 USB. What is the correct one? Answer : "MSP Debug Interface" I had to select this manually.
This made the Cloud IDE work on a Windows 10 machine.
On my primary Windows 7 64-bit machine nothing works....
The desktop version has moved on to another issue.
If I follow this video (looks like a TI video)
https://www.youtube.com/watch?v=JfXz3x1tQFA
I get this message:
Message box title Launching Debug Session
Load program Error.
File: C:\Source\MSP430\TestProject\test\Debug\test.out: Load failed.
Console:
MSP430: Trouble Writing Memory Block at 0xc000 on Page 0 of Length 0x1de: Read timed out
MSP430: File Loader: Verification failed: Target failed to write 0xC000
MSP430: GEL: File: C:\Source\MSP430\TestProject\test\Debug\test.out: Load failed.
Port settings are 9600, 8, None, 1, None
The Cloud running the same code gives this error:
Unable to connect to Launchpad w/ msp430g2553 (16MHz).
Please unplug and re-plug the USB connection and try again.
TI MSP430 USB/MSP430
Error Initializing emulator:No USB FET was found
I am more focused on using the standard desktop version any help would be appreciated.