This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After building , running the code on MSP432P401R gives error.

Other Parts Discussed in Thread: ENERGIA

Hi everyone,

I was working with msp432 and it was working fine ( few example codes). Suddenly, Msp432 is building without any errors but while debugging it gives error.

the error is given below

Error connecting to the target:
(Error -1063 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver.
(Emulation package 6.0.222.0)

I also tried in other ide like energia, still the same error comes.

It was working fine before .

Kindly help me in this regard.

Thanks ,

Andrew Gigie

**Attention** This is a public forum