This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC430F5137 and RTC3 Errata

Other Parts Discussed in Thread: CC430F5137, MSP430F5438

Hi,

I am using CC430F5137 with RTC Module affected by RTC3 errata.

Workaround ASM file found in MSP430F5438 Code Example slac166 starts at 0x5C00 address, out of CC430F5137 flash.

May I move ORG address to 0x8000 without affecting function and alignment of workaround? 

Regards,

Goran

  • Hi Goran,

    Yes, it is advised that you move the ORG address to 0x8000 such that the code is placed in the main memory of the CC430F5137 device. With the CCS version of the RTC workaround this is done automatically depending on the MSP430 device derivative used.

    Regards,
    Ryan

**Attention** This is a public forum