This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG self test fail - Access to LCD RAM

Hi Team,

 

I have a distributor trying to prove if an MSP-GANG is defective and has an error that I have never seen, nor able to find any posts about. Its failing line 205 and 206 of the self test with the explanation of: Access to LCD RAM. Please see the attached full self test dump as well.

=== MSP-GANG Self test results ( Tuesday, August 23, 2016,  14:21:35 ) ===

Adapter SN ------:  15120803 
Hardware --------:  G430:  01.04
Access key ------:  MSP-GANG Programmer 
Silicon Number --:  D40E 916F 2000 1000
API Firmware ----:  MSP-Gang   A430:  01.02.05.00
BOOT Firmware ---:  G430BOOT   B430:  01.00.02.00
GUI Software ----:  MSP-Gang-GUI   G430:  01.02.05.00
DLL Software ----:  MSP-Gang-DLL   D430:  01.02.05.00

================ Test results =============


No.       name                   parameter       limits               result         status


  1: Data Bus   (ALL LOW)          0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
  2: Data Bus   (ALL HIGH)         0x00FF   (0xFFFF  - 0xFFFF)  Result:  0xFFFF   ... >>  OK   <<
  3: Data Bus   (D-0 HI )          0x0001   (0x0101  - 0x0101)  Result:  0x0101   ... >>  OK   <<
  4: Data Bus   (D-1 HI )          0x0002   (0x0202  - 0x0202)  Result:  0x0202   ... >>  OK   <<
  5: Data Bus   (D-2 HI )          0x0004   (0x0404  - 0x0404)  Result:  0x0404   ... >>  OK   <<
  6: Data Bus   (D-3 HI )          0x0008   (0x0808  - 0x0808)  Result:  0x0808   ... >>  OK   <<
  7: Data Bus   (D-4 HI )          0x0010   (0x1010  - 0x1010)  Result:  0x1010   ... >>  OK   <<
  8: Data Bus   (D-5 HI )          0x0020   (0x2020  - 0x2020)  Result:  0x2020   ... >>  OK   <<
  9: Data Bus   (D-6 HI )          0x0040   (0x4040  - 0x4040)  Result:  0x4040   ... >>  OK   <<
 10: Data Bus   (D-7 HI )          0x0080   (0x8080  - 0x8080)  Result:  0x8080   ... >>  OK   <<

 11: Data-2 Bus  (ALL LOW)         0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
 12: Data-2 Bus  (ALL HIGH)        0x00FF   (0xFFFF  - 0xFFFF)  Result:  0xFFFF   ... >>  OK   <<
 13: Data-2 Bus  (D2-0 HI )        0x0001   (0x0101  - 0x0101)  Result:  0x0101   ... >>  OK   <<
 14: Data-2 Bus  (D2-1 HI )        0x0002   (0x0202  - 0x0202)  Result:  0x0202   ... >>  OK   <<
 15: Data-2 Bus  (D2-2 HI )        0x0004   (0x0404  - 0x0404)  Result:  0x0404   ... >>  OK   <<
 16: Data-2 Bus  (D2-3 HI )        0x0008   (0x0808  - 0x0808)  Result:  0x0808   ... >>  OK   <<
 17: Data-2 Bus  (D2-4 HI )        0x0010   (0x1010  - 0x1010)  Result:  0x1010   ... >>  OK   <<
 18: Data-2 Bus  (D2-5 HI )        0x0020   (0x2020  - 0x2020)  Result:  0x2020   ... >>  OK   <<
 19: Data-2 Bus  (D2-6 HI )        0x0040   (0x4040  - 0x4040)  Result:  0x4040   ... >>  OK   <<
 20: Data-2 Bus  (D2-7 HI )        0x0080   (0x8080  - 0x8080)  Result:  0x8080   ... >>  OK   <<

 21: Vcc Target-1 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.02 V   ... >>  OK   <<
 22: Vcc Target-2 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
 23: Vcc Target-3 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
 24: Vcc Target-4 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
 25: Vcc Target-5 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
 26: Vcc Target-6 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
 27: Vcc Target-7 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<
 28: Vcc Target-8 (ALL OFF)         0.00 V  (  0.00 to   0.30)  Result:  0.01 V   ... >>  OK   <<

 29: Translators VT (OFF)           0.00 V  (  0.00 to   0.50)  Result:  0.01 V   ... >>  OK   <<
 30: Translators VT (ON 1.8V)       1.80 V  (  1.60 to   2.00)  Result:  1.78 V   ... >>  OK   <<
 31: Translators VT (ON 2.7V)       2.70 V  (  2.50 to   2.90)  Result:  2.66 V   ... >>  OK   <<
 32: Translators VT (ON 3.6V)       3.60 V  (  3.40 to   3.80)  Result:  3.55 V   ... >>  OK   <<

 33: Vpp Voltage-in                10.00 V  (  8.00 to  12.00)  Result: 10.69 V   ... >>  OK   <<
 34: Vpp Voltage                    7.00 V  (  6.50 to   7.30)  Result:  6.87 V   ... >>  OK   <<
 35: Internal Vcc-3.3V              3.30 V  (  3.20 to   3.40)  Result:  3.30 V   ... >>  OK   <<

 36: Vcc Target-1 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.82 V   ... >>  OK   <<
 37: Vcc Target-2 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
 38: Vcc Target-3 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.79 V   ... >>  OK   <<
 39: Vcc Target-4 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
 40: Vcc Target-5 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.82 V   ... >>  OK   <<
 41: Vcc Target-6 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
 42: Vcc Target-7 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
 43: Vcc Target-8 (ALL ON 1.8V)     1.80 V  (  1.60 to   2.00)  Result:  1.80 V   ... >>  OK   <<
 44: Vcc Target-1 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.70 V   ... >>  OK   <<
 45: Vcc Target-2 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
 46: Vcc Target-3 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.68 V   ... >>  OK   <<
 47: Vcc Target-4 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
 48: Vcc Target-5 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
 49: Vcc Target-6 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
 50: Vcc Target-7 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.69 V   ... >>  OK   <<
 51: Vcc Target-8 (ALL ON 2.7V)     2.70 V  (  2.50 to   2.90)  Result:  2.68 V   ... >>  OK   <<
 52: Vcc Target-1 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.59 V   ... >>  OK   <<
 53: Vcc Target-2 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.58 V   ... >>  OK   <<
 54: Vcc Target-3 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.58 V   ... >>  OK   <<
 55: Vcc Target-4 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.59 V   ... >>  OK   <<
 56: Vcc Target-5 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.59 V   ... >>  OK   <<
 57: Vcc Target-6 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.58 V   ... >>  OK   <<
 58: Vcc Target-7 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.60 V   ... >>  OK   <<
 59: Vcc Target-8 (ALL ON 3.6V)     3.60 V  (  3.40 to   3.80)  Result:  3.58 V   ... >>  OK   <<

 60: Vcc discharge (100ms)Target-1  3.60 V  (  1.00 to   2.70)  Result:  1.18 V   ... >>  OK   <<
 61: Vcc discharge (100ms)Target-2  3.60 V  (  1.00 to   2.70)  Result:  1.15 V   ... >>  OK   <<
 62: Vcc discharge (100ms)Target-3  3.60 V  (  1.00 to   2.70)  Result:  1.18 V   ... >>  OK   <<
 63: Vcc discharge (100ms)Target-4  3.60 V  (  1.00 to   2.70)  Result:  1.14 V   ... >>  OK   <<
 64: Vcc discharge (100ms)Target-5  3.60 V  (  1.00 to   2.70)  Result:  1.17 V   ... >>  OK   <<
 65: Vcc discharge (100ms)Target-6  3.60 V  (  1.00 to   2.70)  Result:  1.17 V   ... >>  OK   <<
 66: Vcc discharge (100ms)Target-7  3.60 V  (  1.00 to   2.70)  Result:  1.15 V   ... >>  OK   <<
 67: Vcc discharge (100ms)Target-8  3.60 V  (  1.00 to   2.70)  Result:  1.13 V   ... >>  OK   <<

 68: Vcc Target-1 ( #1 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.29 V   ... >>  OK   <<
 69: Vcc Target-2 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
 70: Vcc Target-3 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 71: Vcc Target-4 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 72: Vcc Target-5 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 73: Vcc Target-6 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 74: Vcc Target-7 ( #1 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.14 V   ... >>  OK   <<
 75: Vcc Target-8 ( #1 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 76: Vcc Target-1 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
 77: Vcc Target-2 ( #2 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<
 78: Vcc Target-3 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 79: Vcc Target-4 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 80: Vcc Target-5 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 81: Vcc Target-6 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 82: Vcc Target-7 ( #2 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.14 V   ... >>  OK   <<
 83: Vcc Target-8 ( #2 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 84: Vcc Target-1 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
 85: Vcc Target-2 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 86: Vcc Target-3 ( #3 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.27 V   ... >>  OK   <<
 87: Vcc Target-4 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
 88: Vcc Target-5 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 89: Vcc Target-6 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 90: Vcc Target-7 ( #3 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.14 V   ... >>  OK   <<
 91: Vcc Target-8 ( #3 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 92: Vcc Target-1 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
 93: Vcc Target-2 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 94: Vcc Target-3 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 95: Vcc Target-4 ( #4 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.29 V   ... >>  OK   <<
 96: Vcc Target-5 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
 97: Vcc Target-6 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
 98: Vcc Target-7 ( #4 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.14 V   ... >>  OK   <<
 99: Vcc Target-8 ( #4 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
100: Vcc Target-1 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
101: Vcc Target-2 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
102: Vcc Target-3 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
103: Vcc Target-4 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
104: Vcc Target-5 ( #5 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.29 V   ... >>  OK   <<
105: Vcc Target-6 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
106: Vcc Target-7 ( #5 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.14 V   ... >>  OK   <<
107: Vcc Target-8 ( #5 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
108: Vcc Target-1 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
109: Vcc Target-2 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
110: Vcc Target-3 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
111: Vcc Target-4 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
112: Vcc Target-5 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
113: Vcc Target-6 ( #6 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<
114: Vcc Target-7 ( #6 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
115: Vcc Target-8 ( #6 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
116: Vcc Target-1 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
117: Vcc Target-2 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
118: Vcc Target-3 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
119: Vcc Target-4 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
120: Vcc Target-5 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
121: Vcc Target-6 ( #7 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
122: Vcc Target-7 ( #7 ON )         0.00 V  (  3.10 to   3.50)  Result:  3.29 V   ... >>  OK   <<
123: Vcc Target-8 ( #7 ON )         3.30 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
124: Vcc Target-1 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.16 V   ... >>  OK   <<
125: Vcc Target-2 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
126: Vcc Target-3 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
127: Vcc Target-4 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
128: Vcc Target-5 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
129: Vcc Target-6 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
130: Vcc Target-7 ( #8 ON )         0.00 V  (  0.00 to   0.50)  Result:  0.15 V   ... >>  OK   <<
131: Vcc Target-8 ( #8 ON )         3.30 V  (  3.10 to   3.50)  Result:  3.28 V   ... >>  OK   <<

132: SD Power OFF                  0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<
133: SD Power ON                   0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
134: SD Discharge -  delay 2ms     0x0010   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
135: SD Discharge -  delay 50ms    0x0010   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<

136: BSL RX bus (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
137: BSL RX bus (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
138: BSL RX bus (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
139: BSL RX bus (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
140: BSL RX bus (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
141: BSL RX bus (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
142: BSL RX bus (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
143: BSL RX bus (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

144: BSL TX bus (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
145: BSL TX bus (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
146: BSL TX bus (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
147: BSL TX bus (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
148: BSL TX bus (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
149: BSL TX bus (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
150: BSL TX bus (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
151: BSL TX bus (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

152: TDI bus  (#1 HIGH)            0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
153: TDI bus  (#2 HIGH)            0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
154: TDI bus  (#3 HIGH)            0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
155: TDI bus  (#4 HIGH)            0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
156: TDI bus  (#5 HIGH)            0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
157: TDI bus  (#6 HIGH)            0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
158: TDI bus  (#7 HIGH)            0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
159: TDI bus  (#8 HIGH)            0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

160: TDOI Tx-bus (#1 HIGH)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
161: TDOI Tx-bus (#2 HIGH)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
162: TDOI Tx-bus (#3 HIGH)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
163: TDOI Tx-bus (#4 HIGH)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
164: TDOI Tx-bus (#5 HIGH)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
165: TDOI Tx-bus (#6 HIGH)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
166: TDOI Tx-bus (#7 HIGH)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
167: TDOI Tx-bus (#8 HIGH)         0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

168: TDOI Tx-Rx (#1 HIGH)          0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
169: TDOI Tx-Rx (#2 HIGH)          0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
170: TDOI Tx-Rx (#3 HIGH)          0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
171: TDOI Tx-Rx (#4 HIGH)          0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
172: TDOI Tx-Rx (#5 HIGH)          0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
173: TDOI Tx-Rx (#6 HIGH)          0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
174: TDOI Tx-Rx (#7 HIGH)          0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
175: TDOI Tx-Rx (#8 HIGH)          0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

176: TDOI Rx-bus (#1 HIGH)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
177: TDOI Rx-bus (#2 HIGH)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
178: TDOI Rx-bus (#3 HIGH)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
179: TDOI Rx-bus (#4 HIGH)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
180: TDOI Rx-bus (#5 HIGH)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
181: TDOI Rx-bus (#6 HIGH)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
182: TDOI Rx-bus (#7 HIGH)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
183: TDOI Rx-bus (#84 HIGH)        0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

184: TMS bus (All HIGH)            0x00FF   (0x00FF  - 0x00FF)  Result:  0xFF     ... >>  OK   <<
185: TMS bus (All LOW)             0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<

186: TMS bus (#1 HIGH)             0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
187: TMS bus (#2 HIGH)             0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
188: TMS bus (#3 HIGH)             0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
189: TMS bus (#4 HIGH)             0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
190: TMS bus (#5 HIGH)             0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
191: TMS bus (#6 HIGH)             0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
192: TMS bus (#7 HIGH)             0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
193: TMS bus (#8 HIGH)             0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

194: RST bus (All HIGH)            0x00FF   (0x00FF  - 0x00FF)  Result:  0xFF     ... >>  OK   <<
195: RST bus (All LOW)             0x0000   (0x0000  - 0x0000)  Result:  0x00     ... >>  OK   <<

196: RST bus (#1 HIGH)             0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
197: RST bus (#2 HIGH)             0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
198: RST bus (#3 HIGH)             0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
199: RST bus (#4 HIGH)             0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
200: RST bus (#5 HIGH)             0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
201: RST bus (#6 HIGH)             0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
202: RST bus (#7 HIGH)             0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
203: RST bus (#8 HIGH)             0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

204: Keys buffer (All pull-up)     0x001F   (0x001F  - 0x001F)  Result:  0x1F     ... >>  OK   <<

205: Access to LCD RAM (0xAA)      0x00AA   (0x00AA  - 0x00AA)  Result:  0x2A     ... >> ERROR <<
206: Access to LCD RAM (0x99)      0x0099   (0x0099  - 0x0099)  Result:  0x19     ... >> ERROR <<

207: Image Flash Access (get ID)   0x0002   (0x0001  - 0x0003)  Result:  0x01     ... >>  OK   <<

208: TDI Fuse keys (#1 ON)         0x0001   (0x0001  - 0x0001)  Result:  0x01     ... >>  OK   <<
209: TDI Fuse keys (#2 ON)         0x0002   (0x0002  - 0x0002)  Result:  0x02     ... >>  OK   <<
210: TDI Fuse keys (#3 ON)         0x0004   (0x0004  - 0x0004)  Result:  0x04     ... >>  OK   <<
211: TDI Fuse keys (#4 ON)         0x0008   (0x0008  - 0x0008)  Result:  0x08     ... >>  OK   <<
212: TDI Fuse keys (#5 ON)         0x0010   (0x0010  - 0x0010)  Result:  0x10     ... >>  OK   <<
213: TDI Fuse keys (#6 ON)         0x0020   (0x0020  - 0x0020)  Result:  0x20     ... >>  OK   <<
214: TDI Fuse keys (#7 ON)         0x0040   (0x0040  - 0x0040)  Result:  0x40     ... >>  OK   <<
215: TDI Fuse keys (#8 ON)         0x0080   (0x0080  - 0x0080)  Result:  0x80     ... >>  OK   <<

216: TEST Fuse keys (All OFF )      0.00    (  0.00 to   0.30)  Result:  0.00     ... >>  OK   <<
217: TEST Fuse keys (#1 ON)         1.00    (  0.80 to   3.00)  Result:  1.51     ... >>  OK   <<
218: TEST Fuse keys (#2 ON)         2.00    (  0.80 to   3.00)  Result:  1.60     ... >>  OK   <<
219: TEST Fuse keys (#3 ON)         3.00    (  0.80 to   3.00)  Result:  1.54     ... >>  OK   <<
220: TEST Fuse keys (#4 ON)         4.00    (  0.80 to   3.00)  Result:  1.40     ... >>  OK   <<
221: TEST Fuse keys (#5 ON)         5.00    (  0.80 to   3.00)  Result:  1.33     ... >>  OK   <<
222: TEST Fuse keys (#6 ON)         6.00    (  0.80 to   3.00)  Result:  1.33     ... >>  OK   <<
223: TEST Fuse keys (#7 ON)         7.00    (  0.80 to   3.00)  Result:  1.31     ... >>  OK   <<
224: TEST Fuse keys (#8 ON)         8.00    (  0.80 to   3.00)  Result:  1.33     ... >>  OK   <<

============== Finished =================================
*  Test failed!!  2 error(s).
=========================================================

Please let me know your thoughts.

 

Thanks,

Billy

  • Hi Billy,

    I'm looking into this one - new error to me as well, so definitely an unusual issue. Can you have the distributor confirm the following as I work with our team on next steps:

    1. Is it only one MSP-GANG that fails this self-test, or multiple?
    2. Is this a new MSP-GANG that was just received, or one that has already been previously working?
    3. When they power up the MSP-GANG, does anything display on the LCD? Does it look normal/match other MSP-GANG units?
    4. Are there any other symptoms observed that led them to running this self-test?

    Regards,
    Katie
  • Hi Katie,

     

    I’m glad I’m not alone knowing nothing about this error! Please see their very to the point responses:

     

    1. Is it only one MSP-GANG that fails this self-test, or multiple?  This is the only one we have here.


    2. Is this a new MSP-GANG that was just received, or one that has already been previously working?  We had the unit for about two months before it failed.


    3. When they power up the MSP-GANG, does anything display on the LCD? Does it look normal/match other MSP-GANG units?  The display is just garbage.


    4. Are there any other symptoms observed that led them to running this self-test?   Couldn’t read the display.

     

     

    Thanks,

    Billy

  • Hi Billy,

    Thanks for the responses - just what I asked for! I'll work with the team to see what else we may need here.

    Regards,

    Katie

  • Hi Billy,

    This is the first time we've seen an LCD issue, so definitely a rare occurrence! Please have the distributor work with TI customer service to get the unit returned for analysis and we'll send them a new one. I'll contact you offline to work out details.

    Regards,

    Katie

**Attention** This is a public forum