Other Parts Discussed in Thread: MSP430F2618, MSP430-FLASHER, MSP-FET
Hey,
I have been using a MSP430F2618 for a project we are working on, While uploading new code the ground wire that goes from the Emulation tool to the board broke. After this i have been getting the following error:
Fri Sep 16, 2016 18:14:19: Firmware version 3.8.0.2
Fri Sep 16, 2016 18:14:19: Interface dll version 3.8.0.2
Fri Sep 16, 2016 18:14:20: Unknown device : (OpenDevice) , Device=MSP430F2618, PwLength=0x0
Fri Sep 16, 2016 18:14:22: Fatal error: Could not find device (or device not supported) Session aborted!
When I turn on the device it seems to still run the code that was already previously installed onto it, but when I try to upload new code to the controller, it keeps giving that error.
Is the fuse blown or is there anyway to fix this microcontroller to get it working?
Thanks,
Wahaj Khan