Other Parts Discussed in Thread: MSP430WARE, MSP430F5529
Hello,
I would like to ask regarding the Mass Storage Examples (MSC) under TI Resource Explorer>MSP430Ware>Libraries>USB Developers Package>Example Projects.
So I've gotten the Single-LUN File System Emulation Project to work. But the SD-Card Reader Project doesn't seem to work.
Details :
1) I do not have the MSP430F5529 USB Experimenter’s Board, hence I am working with a simple own made SD Card Reader. BUT I've checked with the schematics of the experimenter's Board and they are pretty similar (IMPORTANT Connections being the CLK, MISO, MOSI and CS)
2) I downloaded the MSP430 USB Developers Package which I've noticed is the same as the projects under TI Resource Explorer
3) By 'doesn't seem to work' I am referring to the program not sensing the Insertion/Removal of the SD Card, as I assume is what the program does - or did I misunderstand?
4) Do I have to copy the files created with the USB Descriptor Tool anywhere?
Is there anything specific that I might have to change in the program for it to work? Could you maybe provide me with some links regarding the SD Card interface?
Thank you very much in advance for your assistance.