Other Parts Discussed in Thread: MSP430F2619
Hi,
I'm trying to set my ADC to sample at a 40kHz frequency. I saw I should use the timers to do so, so I set the Timer A for 40kHz.
Im not sure if I didn't get to set the timer A in the good way or if its my ADC's configurations that are wrong. The output in Pin 1.0 which I toggle to see the sampling rate is at 27,7kHz...
Im using IAR.
Could you please get a look into my code and point the errors?
#include <msp430F2619.h>
#include <msp430.h>
// Global variables
int adc[10] = {0}; //Sets up an array of 10 integers and zero's the values
int avg_adc = 0; int i=0; unsigned int timerCount = 0;
// Function prototypes
void adc_Setup();
void adc_Sam10();
void main()
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
BCSCTL1 = CALBC1_1MHZ; // Set range
DCOCTL = CALDCO_1MHZ;
BCSCTL2 &= ~(DIVS_3); // SMCLK = DCO = 1MHz
TACCTL0 = CCIE; //Timer A config
TACTL = TASSEL_2 + MC_1;
CCR0 = 25;
P5SEL |= BIT5;
P5DIR |= BIT5;
P6SEL |= BIT3; // ADC input pin P6.3
P1DIR |= BIT1
P1OUT |= BIT1;
adc_Setup(); // Fucntion call for adc_setup
while(1)
{ P1OUT ^= BIT1; //to measure frequence of sampling
adc_Sam10(); // Function call for adc_samp
}
}
// ADC10 interrupt service routine
#pragma vector=ADC12_VECTOR
__interrupt void ADC12_ISR(void)
{
__bic_SR_register_on_exit(CPUOFF); // Clear CPUOFF bit from 0(SR)
}
// ADC set-up function
void adc_Setup()
{
ADC12MCTL0 = INCH_3 + SREF_0;
ADC12CTL1 = CONSEQ_2 + INCH_3 + CSTARTADD_0 + SHP + SHS1 + ADC12SSEL_0;
ADC12CTL0 = INCH_3 + ADC12ON + MSC + SHT0_0;
}
// ADC sample conversion function
void adc_Sam10()
{
ADC12CTL0 |= ENC + ADC12SC; // Enable Conversion and conversion start
}