Other Parts Discussed in Thread: ENERGIA
Hi. Can someone help me with debugging the codes below? It is for toggling between 2 LEDs using Bluetooth operated by a phone app I designed using MIT app inventor. Below consist of 2 separate codes for energia. I use 2 tabs in energia to run both codes simultaneously to make LED1 light up when my click LED1 on my phone app and vice versa for LED2. Thanks in advance.
CODE 1:
void setup()
{
pinMode(39,OUTPUT);
Serial.begin(9600);
Serial1.begin(9600);
}
void loop()
{
while(Serial1.available()>0)
{
char message =Serial1.read();
if(message=='on2')
{
digitalWrite(39,HIGH);
}
else if (message=='off2')
{
digitalWrite(39,LOW);
}
else
{
analogWrite(39,int(message));
}
}
}
CODE 2:
void setup()
{
pinMode(40,OUTPUT);
Serial.begin(9600);
Serial1.begin(9600);
}
void loop()
{
while(Serial1.available()>0)
{
char message =Serial1.read();
if(message=='on1')
{
digitalWrite(40,HIGH);
}
else if (message=='off1')
{
digitalWrite(40,LOW);
}
else
{
analogWrite(40,int(message));
}
}
}