Hi @ all,
I have a problem with the temperature sensor of the cc430F5137
I use the code of the example package but on different temperatures (-20°C to +60°C) the mesured temperature is still different.
After that i add an offset to the value (calibrated on 23°C). No success. e.g. on -20°C the temperature sensor shows -5°C.
The CC430 is a "final" version (not a XC430). May there are no ore bad calibration data in the TLV?
What can I do to get a correct working temperature sensor?
Thanks for help
Rest rgs
Thomas