This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5418A ACLK error



I have a 32.768 KHz oscillator connected to XIN of a MSP4305418A microprocessor. ACLK is set to XT1CLK which is 32.768 KHz.

P7SEL |= 0X01;   // select crystal bypass mode on XT1 pins

USCCTL4 = SELA__XT1CLK | SELS__DCOCLK | SELM__DCOCLK;

UCSCTL5 = DIVA__1 | DIVS__8 | DIVM__1;

UCSCTL6 = XT2OFF | XT1BYPASS;

I programmed timer A to use ACLK / 1. Timer A counts up to 1023 and resets.

TA0CCR0 = 0X03FF;

TA0CCTL0 = CCIE;

TA0CTL = TASSEL0 | MC0;

The interrupt handler toggles an output every time the counter overflows. The frequency of the output should be 16 Hz. I measured XIN and the output with a frequency counter on two MSP4305418A microprocessors.

XIN = 32.76795350 KHz (- 1.4 ppm)

output = 16.00714183 Hz (+ 446 ppm)

XIN = 32.76795848 KHz (- 1.3 ppm)

output = 15.94690128 Hz (- 3319 ppm)

As you can see, XIN is pretty accurate but the output frequency which is toggled by ACLK is inaccurate. One is a little high and the other is very low.

Why so much error?

Thanks.

**Attention** This is a public forum