Hello,
I have an MSP432P401r Launchpad, trying to implement Bsl programming with UART interface . I’m bit confused with examples and applications notes which is available for this purpose. First I found BSL scripter which serves as a communication tool between PC and MSP432P401. But I do have some doubt in the following command.
I found this line in Script example for MSP432 UART BSL.
RX_DATA_BLOCK_32 BlinkLED_MSP432P401R.txt
What is this Hex file ?
Is this file only contains the program which makes LED blink or even something more that is related to BSL ?
Moreover I found some Custom BSL source code. Do I need to consider that code when I’m using BSL scripter if so please explain how to make use it.
And regarding BSL invocations, when it should be done?
Hope so I’m not confusing more. Please do clarify on this.
Thanks in Advance
Regards,
Bala