Other Parts Discussed in Thread: MSP-EXP430FR5969, MSP-EXP430FR4133
Hello,
I'm trying to get a gauge of what type of battery I might need in order to power the MSP430. I haven't picked a specific model yet, so it is somewhat variable, but one of the ratings I've seen is:
- 220 μA / MHz active mode
To get the number of hours a battery will last I believe I would just take [rating in amp hours] / 220uA. If I were to have a battery rated to 220 mAH then this microcontroller would last ~ 1000 hours in active mode. Is "active" mode simply with the chip in active mode while it's idle? 1k hours seems absurdly long for a small battery.
Considerations to ESD and Vcc seem to indicate from the datasheet that current consumption may exceed 220 uA more often than not. http://www.ti.com/lit/ds/symlink/msp430fr2532.pdf
To be more specific I have to drive a potentiometer (with ADC) and a bluetooth module (likely UART). How might I derive the power requirements of the MSP430 for this?
Thanks!