Hello,
I'm running VMWare Workstation on Windows 8. My development virtual machine is XP-SP3. Unfortunately, it appears the MSP drivers (V1.4.0) don't work in this VM. They are loaded by the device manager correctly when the USB cable is plugged in but hang when the driver tries to initialize the interface. They hang either when trying to connect to the Launchpad through the IAR IDE or when trying to program the device using the MSPFlasher program.
I can connect and flash the launchpad through the Windows 8 host just fine.
Has anyone found a way to configure a XP VM to work with the MSP430FR4133 LaunchPad?
Thanks,
- Dave