This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
debugger cannot access target with external or internal supply at 1.80V
it works fine at 3V.
Same problem in JTAG mode.
Is the MSP-FET able to do targets at 1.8V ?
Viggo Joergensen said:debugger cannot access target with external or internal supply at 1.80V
There is no way to enter SBW / JTAG mode on FR devices with 1.8 VCC. It is not related to used FET software / hardware.
I already commented this few times on e2e.
Why is TI not writing this explicitly in their datasheet for the MSP430FR58xx controllers ?
**Attention** This is a public forum