Other Parts Discussed in Thread: ENERGYTRACE
Good afternoon,
my code sleeps and wakes up upon a rising edge interrupt on P3.3 pin :)
The code works when debugged. However, it does NOT when unplugged and I press the reset pin. I have seen similar E2E threads but was not able to apply the solutions there to success. BTW, just ignore the SPI section.
#include "msp.h"
#include <stdint.h>
#define WAKEUP BIT3
#define SPI_CS BIT3
#define BLUE_LED BIT2
#define GREEN_LED BIT1
#define RED_LED BIT0
static uint8_t RXData[100] = { 0 };
volatile uint8_t idx_RXData = 0;
void send_cmd_to_spi(uint8_t, uint8_t);
void boardInit(void);
int main(void) {
WDT_A->CTL = WDT_A_CTL_PW | // Stop WDT
WDT_A_CTL_HOLD;
__delay_cycles(1000000);
// Initialize GPIO and clocks
boardInit();
// Configuring P1 as output and P1.1 (switch) as input with pull-up resistor
P3->SEL0 &= ~WAKEUP;
P3->DIR &= ~WAKEUP;
P3->OUT &= ~WAKEUP;
P3->REN |= WAKEUP;
P3->IFG &= ~WAKEUP;
P3->IES &= ~WAKEUP; /*!< Port Interrupt Edge Select */
P3->IE |= WAKEUP;
// Turn off PSS high-side supervisors
PSS->KEY = PSS_KEY_KEY_VAL;
PSS->CTL0 |= PSS_CTL0_SVSMHOFF;
PSS->KEY = 0;
// Enable all SRAM bank retentions prior to going to LPM3 (Deep-sleep)
SYSCTL->SRAM_BANKRET |= (SYSCTL_SRAM_BANKRET_BNK1_RET
| SYSCTL_SRAM_BANKRET_BNK2_RET | SYSCTL_SRAM_BANKRET_BNK3_RET
| SYSCTL_SRAM_BANKRET_BNK4_RET | SYSCTL_SRAM_BANKRET_BNK5_RET
| SYSCTL_SRAM_BANKRET_BNK6_RET | SYSCTL_SRAM_BANKRET_BNK7_RET);
// Enable global interrupt
__enable_irq();
// Enable Port 1 interrupt on the NVIC
NVIC->ISER[1] = 1 << ((PORT3_IRQn) & 31);
// Enter or Re-enter LPM4.5
// Set the Power Mode 4.5
PCM->CTL0 = PCM_CTL0_KEY_VAL | PCM_CTL0_LPMR__LPM45;
// Do not wake up on exit from ISR
SCB->SCR |= SCB_SCR_SLEEPONEXIT_Msk;
// Setting the sleep deep bit
SCB->SCR |= (SCB_SCR_SLEEPDEEP_Msk);
// some BOOT led (blue)
P2->OUT |= BLUE_LED;
__delay_cycles(1000000);
P2->OUT &= ~BLUE_LED;
// P3.2 as wake-up input pin, clear IFG, enable IE, low-to-high
P3->SEL0 &= ~WAKEUP;
P3->DIR &= ~WAKEUP;
P3->OUT &= ~WAKEUP;
P3->REN |= WAKEUP;
P3->IFG &= ~WAKEUP;
P3->IES &= ~WAKEUP; /*!< Port Interrupt Edge Select */
P3->IE |= WAKEUP;
// ---------------------------- start of spi section ----------------------------------
// Set P1.5 CS low (but is active high)
P1->DIR |= SPI_CS;
P1->OUT &= ~SPI_CS;
__delay_cycles(1000000);
// Set P1.5, P1.6, and P1.7 as SPI pins functionality
P1->SEL0 |= BIT5 | BIT6 | BIT7;
EUSCI_B0->CTLW0 |= EUSCI_B_CTLW0_SWRST; // Put eUSCI state machine in reset
EUSCI_B0->CTLW0 = EUSCI_B_CTLW0_SWRST | // Remain eUSCI state machine in reset
EUSCI_B_CTLW0_MST | // Set as SPI master
EUSCI_B_CTLW0_MSB; // MSB first
// ACLK, /2, fBitClock = fBRCLK/(UCBRx+1), init USCI state machine
EUSCI_B0->CTLW0 |= EUSCI_B_CTLW0_SSEL__ACLK;
EUSCI_B0->BRW = 0x01;
EUSCI_B0->CTLW0 &= ~EUSCI_B_CTLW0_SWRST;
send_cmd_to_spi(0x0a, 0x0b);
// ---------------------------- end of spi section ----------------------------------
__sleep();
__no_operation();
// For debugger
// Blink LED slowly if LPM4.5 not entered properly
while (1) {
P1->OUT ^= BIT0; // XOR P1.0
__delay_cycles(1000000);
}
}
// Port 1 interrupt service routine
void PORT3_IRQHandler(void) {
P1->OUT |= BIT0; // Set P1.0
__delay_cycles(500000);
P1->OUT &= ~BIT0; // Clear P1.0
P3->IFG &= ~WAKEUP; // Clear P1.1 IFG
}
void boardInit(void) {
// GPIO Port Configuration for lowest power configuration
P1->OUT = 0x00;
P1->DIR = 0xFF;
P2->OUT = 0x00;
P2->DIR = 0xFF;
P3->OUT = 0x00;
P3->DIR = 0xFF;
P4->OUT = 0x00;
P4->DIR = 0xFF;
P5->OUT = 0x00;
P5->DIR = 0xFF;
P6->OUT = 0x00;
P6->DIR = 0xFF;
P7->OUT = 0x00;
P7->DIR = 0xFF;
P8->OUT = 0x00;
P8->DIR = 0xFF;
P9->OUT = 0x00;
P9->DIR = 0xFF;
P10->OUT = 0x00;
P10->DIR = 0xFF;
PJ->OUT = 0x00;
PJ->DIR = 0xFF;
}
Have a really nice day. Looking forward to your knowledge.