Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 disabling the MPU

I am using an FR6989 and I configure the MPU at power-up to prevent writes into code space and to execution from data space. This project requires that I allow upgrades through a serial port. I accept the SREC file via the serial port, and write it to an external flash via I2C. Once that is done, I copy a section of code to ram and execute it. This code copies the new code from the external flash to its run-time location in FRAM, then I reboot the processor to start running the updated code. This all worked fine until I started to use the MPU. As I mentioned, I configure and enable the MPU at power-up, then I disable the MPU just before jumping to RAM to do the upgrade. But it seems as though the MPU doesn't get disabled, or it does get disabled, but my code doesn't run. I am assuming that there is some procedure that I need to follow, that I haven't figured out yet. I have found several articles on how to configure the MPU, but nothing about disabling it. I have tried several things but here is the last thing I tried:

   MPUCTL0 = MPUPW; // First, write Password bit to access MPU registers and dissable the MPU

   // Make every section unprotected (just in case I need to do this for the new code to run)            
   MPUSAM = (MPUSEG1WE | MPUSEG2WE | MPUSEG3WE | MPUSEG1RE | MPUSEG2RE | MPUSEG3RE | MPUSEG1XE | MPUSEG2XE | MPUSEG3XE);
  

I also tried locking the MPU and re-starting the MPU after the above, but that seems to make matters worse.

     

  • 
    

    Ronald,

    How do you have your MPU configured? Are you locking the MPU initially? If so, try it without any lock.

    I modified the example code as follows and it protected the address on the line 98 writes, and wrote to the address on line 119.

    Let me know if this helps!



    /* --COPYRIGHT--,BSD_EX * Copyright (c) 2014, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430FR69xx Demo - MPU Write protection violation - Interrupt notification // // Description: The MPU segment boundaries are defined by: // Border 1 = 0x6000 [MPUSEGB1 = 0x0600] // Border 2 = 0x8000 [MPUSEGB2 = 0x0800] // Segment 1 = 0x4400 - 0x5FFF // Segment 2 = 0x6000 - 0x7FFF // Segment 3 = 0x8000 - 0x13FFF // Segment 2 is write protected. Any write to an address in the segment 2 range // causes a PUC. The LED toggles after accessing SYS NMI ISR. // // ACLK = n/a, MCLK = SMCLK = default DCO // // // MSP430FR6989 // --------------- // /|\| | // | | | // --|RST | // | | // | P1.0|-->LED // // William Goh // Texas Instruments Inc. // April 2014 // Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0 //****************************************************************************** #include <msp430.h> unsigned char SYSNMIflag = 0; unsigned int *ptr = 0; unsigned int Data = 0; int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Configure GPIO P1DIR |= BIT0; // Configure P1.0 for LED // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; // Configure MPU MPUCTL0 = MPUPW; // Write PWD to access MPU registers MPUSEGB1 = 0x0600; // B1 = 0x6000; B2 = 0x8000 MPUSEGB2 = 0x0800; // Borders are assigned to segments MPUSAM &= ~MPUSEG2WE; // Segment 2 is protected from write MPUSAM &= ~MPUSEG2VS; // Violation select on write access MPUCTL0 = MPUPW | MPUENA | MPUSEGIE; // Enable MPU protection // MPU registers locked until BOR Data = 0x88; // Cause an MPU violation by writing to segment 2+ ptr = (unsigned int *)0x6002; *ptr = Data; __delay_cycles(100); // while(SYSNMIflag) // Has violation occured due to Seg2 // { // P1OUT ^= BIT0; // Toggle LED // __delay_cycles(100000); // Delay to see toggle // } MPUCTL0 = MPUPW; MPUSAM |= MPUSEG2WE; // Segment 2 is protected from write //MPUSAM |= ~MPUSEG2VS; // Violation select on write access MPUCTL0 = MPUPW | MPUENA | MPUSEGIE; // Enable MPU protection *ptr = Data; // No violation - trap here while(1); } // System NMI vector #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = SYSNMI_VECTOR __interrupt void SYSNMI_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(SYSNMI_VECTOR))) SYSNMI_ISR (void) #else #error Compiler not supported! #endif { switch (__even_in_range(SYSSNIV, SYSSNIV_CBDIFG)) { case SYSSNIV_NONE: break; case SYSSNIV_RES02: break; case SYSSNIV_UBDIFG: break; case SYSSNIV_RES06: break; case SYSSNIV_MPUSEGPIFG: break; case SYSSNIV_MPUSEGIIFG: break; case SYSSNIV_MPUSEG1IFG: break; case SYSSNIV_MPUSEG2IFG: MPUCTL1 &= ~MPUSEG2IFG; // Clear violation interrupt flag SYSNMIflag = 1; // Set flag break; case SYSSNIV_MPUSEG3IFG: break; case SYSSNIV_VMAIFG: break; case SYSSNIV_JMBINIFG: break; case SYSSNIV_JMBOUTIFG: break; case SYSSNIV_CBDIFG: break; default: break; } }

  • Ronald,
    2 other things:
    When it isn't working, what sort of behavior does it exhibit?

    Another thing you could try, is to clear the MPUENA bit before writing the protected memory. That should FULLY disable the MPU. You will need the password to do this.
  • Thanks Cameron, Disabling the MPU fixed the problem.

**Attention** This is a public forum