Other Parts Discussed in Thread: CC3200
Team,
Lots of other Forum posts on this subject. Just want to clarify for our customer.
If the MSP432 is the SPI Master but where some SPI Slaves require 16 bits framing and some Slaves require 8bits framing, is this still supported?
Bus speed remains the same in both cases. The master can adapt the bus speed/framing to what is required for a particular slave, not the other way around obviously. The master needs to be able to support 8bits and 16bits framing for the customer application.
Although the MSP432 SPI implementation is indeed on an 8-bit framing mechanism, we believe that with a SPI Master implementation, both 8 and 16-bit should be possible given One byte after the other…since the Master provides the clock in that case.
Comments welcomed please!
-CY