Hi,
I'm new there. I do a little project in my university and I must be able to power an Arduino with a AGM 12V battery and solar pannel.
I see that the PMP7647 board using the MSP430 could do that
But I don't know if it will work well? The arduino has 2 arducam and 2 led flash. It will consum less than 500mA (in 12V) and my solar pannel would be 5W 12V. I think the PMP7647 is overkill? Did you have other solution to my application?
Does the board interupt the charging wenn the battery voltage reach 14V? Does the board interrupt the load if the voltage is under 12V? It is possible to have a signal wenn the battery is 40% of charge (12.2V) to send a signal for changing the battery?
Thanks for your answer and sorry for my bad english :S