Other Parts Discussed in Thread: MSP430FG4619
I'm using msp430fg4619. I have one question. Is msp430 support RAM external? what msp430 family is supported RAM external?
Thank you very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FG4619
I'm using msp430fg4619. I have one question. Is msp430 support RAM external? what msp430 family is supported RAM external?
Thank you very much.
I would agree it is a bit confusing and it took me a minute to comprehend what is being illustrated.
The MSP430FG4619 has 4K bytes of RAM total on the device (ie. integrated on-chip).
2K bytes @ 0x0200 through 0x09FF (this is mirrored @ 0x1100 through 0x18FF)
2K bytes @ 0x1900 through 0x20FF
Mirrored RAM happens, if an MSP has more ram than his smaller brothers, yet needs this ram to be moved to a different address because on the original address is not enough space for the whole amount. Then part of this ram is mirrored to the original location, so that the MSP is binary backwards compatible to the smaller MSPs.
In case of the 4619, from the 4k RAM (which are located on the area 0x1100-0x20ff), the lower 2k are mirrored to the area 0x0200-0x09ff where some smaller MSPs have their 2k ram. Since right above this area the boot memory is located, the ram couldn't be just enlarged.
Since the ram should be in a continuous block, it had to be moved. Yet part of it is mirrored to the 'old' location, so code written for the smaller MSP will also run on the bigger one, which has the same (and more) hardware modules, ports etc, so it can be used as replacement.
There is, however, no externally available data or address bus, so no external ram can be attached to the MSP (other than under program control as 2nd level memory like SD card or HD or whatever.)
**Attention** This is a public forum