Other Parts Discussed in Thread: MSP430F6736, TIDM-SERVER-PWR-MON, TM4C1294NCPDT
Hello,
We would like to use Energy metering solution for energy monitoring in our product.
The product is used indoor or outdoor. It is required to measure the energy consumption of a Device that has AC Power supply input. An AC to DC Power module is used to generated DC voltage (constant current output 1A and voltage varying from 52V to 62V, without load the Voltage can go upto 69V.
The requirement is to measure the total energy consumed by this product and should be displayed.
The query is Whether to use the Energy metering IC on AC "Input side" or on the DC Output "Load side".
refered to SLAA517E application report "Implementation of a Single-Phase Electronic Watt-Hour Meter Using the MSP430F6736(A)"
Regards,
Sumathi