This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART on the programmer side is not working (MSP430G2553 Launchpad)

Other Parts Discussed in Thread: MSP430G2553

Hi,

The UART on the MSP430G2553 Launchpad stopped out of the sudden, apparently, the problem isn't from the MCU because I tested the UART on-chip and it's working fine, the issue is with the UART in the programmer side, it doesn't communicate anymore with the MCU. Any clue why this would happen?

Note: all jumpers are in the right place, the board used to work normally till recently, still the programmer works and I can upload any code to the MCU without any issues, only the communication using the UART of the programmer is down.

Cheers.

**Attention** This is a public forum