This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestion for 32Bit microcontroller

Hello,

Can anyone suggest me good 32-bit microcontrollers? Criteria for selection are as following:

1. Must have a compact size.

2. Having less number of Pins.

3. More than 16 MHz clock.

4. 32-bit architecture 

Thank you.

Best Regards,

Dinesh Jinjala.

**Attention** This is a public forum