This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

warning :#17003-D relocation from function

Other Parts Discussed in Thread: MSP430F5438A, MSP430F5437A

Hello,

 

I work with the msp430f5438A , and compile with CCS 5.3 .

When I compile with large memory and code model I get the warning:

#17003-D relocation from function.

The warning is point to the code, where is a large array ( look up table) .

And the warning :

#10015-D output file…. Cannot be loaded.

 

All the array defined with const type qualifier.

 

The questions:

  1. due the fact that I use large data model and large code model. How can I get warning of relocation from function?
  2. How can I solve that warning?

 

compiler setting:

-vmspx --abi=eabi --code_model=large --data_model=large -g --include_path="C:/ti/ccsv5/ccs_base/msp430/include" --include_path="C:/ti/ccsv5/tools/compiler/msp430_4.1.2/include" --include_path="../hal" --include_path="../impact" --include_path="../hdr" --advice:power="all" --define=__MSP430F5437A__ --define=_LARGE_MEMORY_MODEL_ --define=_OPR_ --diag_warning=225 --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU23 --silicon_errata=CPU40

 

linker setting:

-vmspx --abi=eabi --code_model=large --data_model=large -g --advice:power="all" --define=__MSP430F5437A__ --define=_LARGE_MEMORY_MODEL_ --define=_OPR_ --diag_warning=225 --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU23 --silicon_errata=CPU40 -z --stack_size=400 -m"../Release/kela_ver_x_x.map" --heap_size=400 --use_hw_mpy=F5 -i"C:/ti/ccsv5/ccs_base/msp430/include" -i"C:/ti/ccsv5/tools/compiler/msp430_4.1.2/lib" -i"C:/ti/ccsv5/tools/compiler/msp430_4.1.2/include" --reread_libs --warn_sections --display_error_number --rom_model

 

Thanks.

 

**Attention** This is a public forum