Hello,
I am trying to establish communication with the MSP430FR2532 on my target board using the Spy-Bi-Wire interface, the MSP-FET programmer and Elprotronic Lite application. When trying to "Verify Security Fuse" in Elpotronic software, I get an error that says that the: Target Microcontroller is not responding. The same error happens when trying to debug using CCS 6.2. I tried multiple voltages with the same result.
Here's my schematic :
I hand-soldered the components and tried multiple boards with the same result. The one show in the pictures below has only the minimal components soldered: the MCU, C6, C7, R6 and C8. Note that the capacitive pull-down C11 is not soldered.
I checked the continuity from one end of the programmer's ribbon cable to the board connections and it looks fine. I also checked the voltage supplied.
I'm kind of desperate here since I tried every lead I thought of. Thanks for your help !