This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BSL gives error- > [ACK_ERROR_MESSAGE]Packet Size exceeds maximum buffer size!

Other Parts Discussed in Thread: MSP430F5310

Hi,

I'm trying to program the MSP430F5310 through the BSL.

I use CCS6.2 to generate the intel .HEX file and TI.TXT file.

When I run the script, the TI.TXT file works fine, but the intel .HEX file gives the error:

[ACK_ERROR_MESSAGE]Packet Size exceeds maximum buffer size!

Refer to the attached log-files.

Is there something wrong with the .HEX file generated by the CCS6.2?

Kind regards,

Ben

**Attention** This is a public forum