Other Parts Discussed in Thread: MSP430F2013, OPA333
Hi
I am developing a digital weight scale using TI OPA333, MSP430F2013 and tps71533. What I am seeing is the OPA333 doesn't give stable output with variation in temperature.
If I vary the temperature from 26 degrees to 60 degrees the output of the opamp is as follows
26 degrees - 264
35 degrees- 262
40 degrees - 258
45 degrees - 262
55 degrees - 264
The worst part is the reading is not the same when the temperature rises from 26 to 55. I mean I am getting different readings when the temperature rises from 26 to 55.
These readings are not the same as when the temperature falls from 55 to 26.
Any idea how to fix this problem
Thanks in advance
Kind regards
Suchitra