HI
I'm using MSP-Gang 1.2.5. there is a C# demo in installed dir .
C:\Program Files (x86)\Texas Instruments\MSP-GANG\Examples\C#_MSP_DLL
When I using Visual Studio 2015 open and upgrade the Solution, the project can not be Build.
--------------------------------------
public struct DATA_BUFFERS
{
byte[] SourceCode = new byte [DBUFFER_SIZE]; //source code from the file
byte[] UsedCode = new byte [DBUFFER_SIZE]; //combined data (source code, serialization etc)
byte[] CommonTx = new byte [DBUFFER_SIZE]; //data used to writing - the same data to all targets
byte[][] GangTx = new byte [DBUFFER_SIZE][GANG_SIZE]; //selective data used to writing
byte[][] GangRx = new byte [DBUFFER_SIZE][GANG_SIZE]; //data read from all targets
byte[] Tmp = new byte [DBUFFER_SIZE];
byte[][] JTAG_Passsword = new byte [2][JTAG_PASSW_LEN];
byte[][] BSL_Passsword = new byte [2][BSL_PASSW_LEN];
byte[] Flag_ScrCode = new byte [DBUFFER_SIZE]; //0 - empty 1-Code1, 2-Code2, 4-Appended Code in SourceCode[x];
// #define CODE1_FLAG 1
// #define CODE2_FLAG 2
// #define APPEND_CODE_FLAG 4
byte[] Flag_UsedCode = new byte [DBUFFER_SIZE]; //0 - empty 1-valid data in UsedCode[x];
byte[] Flag_WrEn = new byte [DBUFFER_SIZE]; //0 - none 1-write/verify enable in FlashMem[x]
byte[] Flag_EraseEn = new byte [DBUFFER_SIZE]; //0 - none 1-erase enable in FlashMem[x]
byte[] Flag_RdEn = new byte [DBUFFER_SIZE]; //0 - none 1-read enable in FlashMem[x]
byte[] Flag_Sp1 = new byte [DBUFFER_SIZE]; //spare
byte[] Flag_Sp2 = new byte [DBUFFER_SIZE]; //spare
byte[] Flag_Sp3 = new byte [DBUFFER_SIZE]; //
byte[][] Flag_JTAG_Passw = new byte [2][JTAG_PASSW_LEN]; // [0][..]-password from code file; [1][..]-password from password file
byte[][] Flag_BSL_Passw = new byte [2][BSL_PASSW_LEN]; // [0][..]-password from code file; [1][..]-password from password file
}
-----
Every line show the exception:
Severity Code Description Project File Line Suppression State
Error CS0178 Invalid rank specifier: expected ',' or ']' SimpleMSP-GANG C:\Program Files (x86)\Texas Instruments\MSP-GANG\Examples\C#_MSP_DLL\MSP-GANG-Dll.cs 419 Active