Tool/software: Code Composer Studio
Hellow all.
Before using the 'MSP-FET430UIF' I have not had a problem, use this time to a new 'MSP-FET Flash Emulation Tool' purchase has the problem occurs below.
There is nothing wrong with the USB and the device we received, and it seems that there is no problem connecting to the MCU through the JTAG connection.
I think the voltage of 3V is not being input to the equipment. Is it necessary to input the setting separately in 'MSP-FET Flash Emulation Tool'? Or, I'm running a firmware upgrade using 'MSPFlasher', do I need to change the 'MSPFlasher' settings?
ERROR is 'Uknown device'... why this ERROR is showing.
if someone have solution at this situation. please tell me.
thanks.