This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2311: Correct way to reset SPI slave state machine

Part Number: MSP430FR2311


I have an MSP430FR2311 operating as an SPI slave. It is working correctly. My question is about how to properly handle error cases when the incoming master data is incorrect. Specifically, how to properly handle the case where the master only clocks out 7 bits during a chip-select cycle, when the MSP is configured for 8 bits.

I have a test case where the master clocks out only 7 bits (an erroneous condition) during one chip-select cycle (STE is released after the seventh bit). The master then starts a new chip-select cycle and clocks out the correct number of bits (8) and I expect the byte value received by the MSP slave to be the value in that second set of 8 bits. What I'm seeing is the received value is a combination of the 7 bits from the first CS cycle, and the first bit from the second CS cycle. I understand why this is happening, the SPI slave state machine doesn't reset its shift register just because CS is de-asserted. The question I have is, what is the correct way to force the slave's state machine to reset so that in this second CS cycle the correct data is read?

I have tried setting and then clearing the RST bit in the CTLW0 register (I don't have the exact register name handy here at home -- it's bit zero of the first SPI register) but that doesn't seem to work. When I do this, I don't get an SPI receive interrupt during the second CS cycle, where I expect to get one interrupt.

Is this the right approach, or is there another way to reset the slave state machine?

  • Hi Richard.

    In an application like yours I did exactly the same, one pin was a "chip select" pin that was controlled by the master MSP430. Whenever it was driven high, I reseted the USCI module by setting the UCSWRST bit. When the master pulled chip select low, the USCI module was activated again by clearing the bit. I never had any problems, the state machine was reset every time. But I did not use STE, I used a GPIO pin with interrupt. Inside the interrupt I configured the USCI module.

    Dennis

  • Section 22.3.1 of the User's Guide says:

    When set, the UCSWRST bit resets the UCRXIE, UCTXIE, UCRXIFG, UCOE, and UCFE bits, and sets the UCTXIFG flag.

  • Thanks, good to know this worked for you. This prompted me to look elsewhere for the problem.
    My problem was that I needed to re-configure the SPI peripheral after cycling the RST bit. This wasn't clear from the data sheet or user guide, but once I started doing that it worked fine.
  • I must be missing something in your answer ...? Which of these bits is associated with the shift register / state machine?

**Attention** This is a public forum